Browse FAQs



Galaxy 3500, Smart-UPS VT and ais3000 Power Factor Information
Galaxy 3500 , Smart- UPS VT and ais3000 Power Factor Information ... Galaxy 3500 , Smart- UPS VT and ais3000 ... Galaxy 3500 , Smart- UPS VT and ais3000 Power Factor Information ... "The SUVT and the ais3000 have an Input Power Factor Correction Module which corrects the Power Factor on the input of the unit. The Input Power Factor is 1 . The Output Power Factor is 0.8 - what means that, for example, a 10kva unit can provide a maximum total load of 8KW. This means there is a difference of 20 % between real and apparent power.
Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries
... used in PX1 20 ,40, ... 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and ... 250/500kva UPS units) batteries ...
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
Smart- UPS VT- Galaxy 3500 ; Bypass Not ... Smart- UPS VT- Galaxy 3500 -ais3000 ... occurs when the UPS is online, ... , the UPS should not allow ... to command the UPS to bypass. If the UPS allows you to ... are displayed for 20 > seconds) ... ... window, the UPS should be in ... 60 HZ +/- 0, 1 % ... 50 HZ +/- 0, 1 % ... When AC mains returns you may get a informational event for; Mains no longer prevents UPS from switching to bypass.
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
Galaxy 3500 , SUVT , EPO, REPO, g3500, Battery frame, XR frame, XR frame EPO circuit wiring, Installation – ...
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
g3500, galaxy 3500 , SUVT , accessories, MGE g3500, MGE galaxy 3500 , SmartSlot accessories, AP9622, modbus
What UPS units are officially supported by the ap9610 (Relay I/O SmartSlot Card)?
SURTA SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)
What UPS units are officially supported by the AP9613 (Dry Contact I/O SmartSlot Card)?
SURTD SUVT / Galaxy 3500 (Must use Configuration #2 - same as Symmetra)
Smart-UPS VT and Galaxy 3500 Power Off, Bypass and Power on Procedures
SUVT , Galaxy 3500 , Smart- UPS VT, Smart Ups VT,Smart- UPS VT and Galaxy 3500 Power Off, Bypass ...
Smart-UPS VT-g3500; Load does not turn on automatically after an outage/shutdown
Suvt autostart, Galaxy 3500 Autostart, SUVT turn load on, set auto start to on, restart, how to set auto start ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.