Browse FAQs



APC Schneider Cooling Unit Identification
62 (18T) AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) ... CM 003 ( 1 T) ... -230/ 1 /60 ... =277/ 1 /60 1 -5T ... 1 -3T ... ... -230/ 1 /60 ... =277/ 1 /60 ... CM 15 ( 1 T) ... =208/ 1 /60 ... =230/ 1 /60 ... =277/ 1 /60 ... Drycooler 15 ( 1 T) ... =230/ 1 /60 ... = 460/ 1 /60
What are the operational conditions for an InRoom (Stulz) Unit
This document will describe what are the operational conditions for an InRoom (Stulz) Unit. ... The InRoom precision air conditioning units operate within the following ranges: ... Frequency:60 Hz +/- 1 % ... Return air conditions for evaporator capacity ( DX ): 24°C (75°F) 50% R. H. ... Cooling fluid ( DX ): 30% Glycol
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package
Product line: ACRD1XX, ACRD2XX, ACRP1XX, ACRD5XX, Uniflair DX , Network Air FM, InRoom DX .
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... InRoom Direct Expansion ... Installation Services ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Planning Tools and Publications ... PowerChute plus ... Project Management Services ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service ... Training Services
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
PowerChute Plus ... When new versions of software are released, Schneider Electric will continue to provide full technical support to customers for the previous version for a minimum of 1 year after the new version is released. In practice, Schneider Electric typically goes far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes. ... PowerChute Plus (PC+) was discontinued March 2007
Stulz Tech Data Manual
ACPDX21-86, acpcw40-150, Tech Data Manual, Stulz, Chilled Water, Dx , Inroom
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... Static Load Weight Rating is the maximum weight of the cabinet, plus installed equipment (with the feet locked), in it's final location. ... This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Example: a customer who wishes to move a cabinet from one row to another in a data center must remove equipment until the weight is equal to (or below) the Dynamic Load Rating before being moved.
How do I go about Resetting or Reconfiguring my DG5 board.
... : CCT- DX , CCT- ... , AFX- 1 , AFX- ... Ceiling Mount- DX , Ceiling Mount ... , Techcool- DX , Techcool- ...
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... RES CARB FILM 1 /4W ... ROTO MALE STRAIGHT 1 1 /4" - 3/4" SWT - ( DX Refrig
How can I adjust the number of battery packs on a Smart-UPS XL?
To adjust the number of battery packs via a Terminal session: 1 . Unload the PowerChute plus NLM (pwrchute.nlm)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.