Browse FAQs

Does the W870-8135 NetShelter key work on the combination handle AR8132A?

Published date: 19 September 2019

Issue: 
A customer claims that their new AR8132A door handles can be opened with the standard NetShelter 333 key: W870-8135. 

Product Line: 
NetShelter SX, AR8132A

Environment: 
All models, all serial numbers. 

Cause: 
The AR8132A uses a different key, but the standard 333 key will also open the lock. 

Resolution: 
The AR8132A will accept any key similar when the combination is set to the factory default of 000. 
Once a new combination is set, only the key included with the AR8132A will open the lock. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.