Browse FAQs

Video: How to change a Cooling Set point on a push button Uniflair display

Published date: 03 September 2020

Issue:
How to change a cooling set point on a Uniflair Unit.
 
Product line:
All Uniflair Units with Push-Button Display, All Chilled Water Uniflairs.
 
Environment:
All Serial Number with Push-Button Units.
 
Cause:
Repair, Install, Maintenance.
 
Resolution
 
How to change a Cooling Set point on a push button Uniflair display.
 
Press <> PRG.
 
Settings Menu <> ENTER.
 
Code <> 00000 ENTER.
 
Operative settings <> ENTER.
 
Press ENTER again to the cooling set point.
 
Use the Arrows to set the correct temperature.
 
Press ENTER twice and then ESC back out to the main menu.
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.