Browse FAQs

Video: How to change the alarm delays on a Network Air FM unit

Published date: 16 October 2019

Issue:
This document will detail the procedure for how to change the alarm delays on a Network Air FM unit.
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
 
Environment:
All Serial Numbers.
 
Cause:
Install, Configuration.
 
Resolution:
 


To change the alarm delays for temperature and humidity through the front display.
  1. Press ESC key until you get to the main menu.
  2. Then select SETUP and then SYSTEM 1.
  3. Select ALARM and then select ALARM DELAYS.
  4. Now you have a choice of either Temperature or Humidity. Select one by using the UP or DOWN arrows.
  5. Then press ENTER and now you can change the delays times anywhere from 0-999 seconds.
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.