Browse FAQs

Do the NetShelter SX Shock Package cabinets include the OSHPD or IBC High Seismic Area mounting brackets?

Published date: 23 October 2019

Issue:
Preparing for installation, want to know if the pallet brackets from the Shock Packaging can be used to mount the cabinet to the floor.

Product Line:
NetShelter SX Shock Package

Environment:
All versions and serial ranges.

Cause:
Pallet brackets from non-SP cabinet can be used as bolt-down brackets. 

Resolution:
The Shock Package cabinets do not include the seismic mounting brackets. They must be purchased separately.
Please use AR7701A-S as the seismic mounting brackets for NetShelter SX SP-series cabinets into IBC High Seismic Area or OSHPD installatiions.
For installation in IBC Low Seismic Area or Moderate Seismic Area please use either AR7701A-S or AR7701. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.