Browse FAQs

Can I use multiple ACSC1XX units in a single room?

Published date: 17 July 2020

Issue:
This article answers the question of can I use multiple ACSC1XX  units in a single room?

Product line:
ACSC1XX.

Environment:  
All Serial Numbers.

Cause:
FAQ.

Resolution:
Yes, the only limitation is the ability of the ceiling plenum to handle the airflow and heat rejection from the SC units. The SC units now have group controls built into the firmware that allows them to talk to one another.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.