Browse FAQs

AC Cooling equipment: ODC Ozone Depleting Chemicals

Published date: 18 July 2020

Issue:
This is a list of all Cooling units and the type of refrigerant that is used. 

Product line:
All Cooling Units. 

Environment:
All Product models, all serial numbers. 

Cause:
Ozone Depleting Chemicals.

Resolution: 

AC Cooling equipment: ODC Ozone Depleting Chemicals

There is a push from the EPA to move away from ODC’s used in refrigeration. You may be asked, especially from Canada sites, if our systems use ODC. Our current 2012 line of cooling equipment do not use ODC.  However, some of our older systems do use R22 which is considered an ODC.

Which units use R22?

 

AFX, CCT, CM, FM, ACPA4000, and TC all use R22 which is an ODC

 

What other refrigerants do we use that are not ODC?

410a


ACPSCx, ACRD10x, ACSC10x, TDVAx

 

407c
ACRP10x, ACRD50x, ACPDX21-86

 

134a
RDU, OA,

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.