Browse FAQs

Why does PowerChute Business Edition using Simple Signalling and an Active Management Technology serial port cause Immediate Shutdown of Operating System?

Published date: 13 January 2021

Issue:
Installing PowerChute Business Edition using Simple Signaling and an Active Management Technology serial port causes Immediate Shutdown of Operating System (and restarting results in another shutdown).
 
Product Line:
PowerChute Business Edition version 9.1, 9.1.1, 9.2, 9.2.1, 10.0.0, 10.0.1, 10.0.2
 
Environment:
Active Management Technology (AMT) ports. These ports are often available on HP machines.
 
Cause:
The Intel Active Management Technology (AMT) ports are used for Out-of-Band Management.
 
Solution:
Reboot the OS in Windows Safe Mode and then uninstall PowerChute Business Edition. Reinstall PowerChute use another COM port or a USB port.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.