Browse FAQs



How to navigate through an Network Air FM unit display
... NetworkAIR FM DX Precision Air Conditioner . Direct expansion (DX) ... ... capacity uses one compressor and half of ... ... coil and both compressors . ... All refrigerant is directed through the expansion valve which feeds ... ... in which the compressors are engaged to ... hours that each compressor runs. ... in which the compressors are engaged. ... in which the compressors are engaged should ... ... used in the direct expansion refrigeration system. ... ... begins when the compressor engages and then prevents the compressor from disengaging until ... ... It protects the compressors from rapidly cycling ... ... can shorten the compressor life by causing ...
General functions of a MicroAC control platform DG3
... an electronic control for the complete management of precision air-conditioners , both in direct expansion versions (with 1 or 2 compressors ) ...
APC Schneider Cooling Unit Identification
E= Expansion A= Air Cooled E= Air Cooled U= Upflow R= Upflow U= Upflow R= Upflow ... Main A= Air Cooled U= Upflow ... ) A= Air Cooled U= Upflow R= Upflow ... ) A= Air Cooled UD= Upflow ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... ... -5T Air Cooled or ... 0 A= Air Cooled SC= Air Cooled Self-Contained IR= Air Cooled Indoor Condenser IG= Air Cooled Indoor Condensing
What are the operational conditions for an InRoom (Stulz) Unit
The InRoom precision air conditioning units operate within the following ranges: ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) ... Upflow units with an external static pressure: 50 Pa (0.20 in w g)
What is meant by ‘flooding’ with Air Conditioners?
All A/C Units with Compressors . ... Flooding (also known as ‘flood back’) is the term used to describe the condition when Liquid refrigerant reaches the compressor . ... Flood back of refrigerant to the compressor (low superheat) is defined as liquid refrigerant reaching the compressor . ... • Evaporator fans not operating.
DAC, Cancoil Installation Manual
Air Cooled Condenser DAC Air Cooled Condensers For information ... Cancoil air-cooled condensers have been ... ... be used if air-cooled quipment is located ... ... ventilation) per compressor horsepower must be ... ... down to the compressor . ... systems with parallel compressors or systems with ... ... column to the expansion valve. ... return to the compressor . Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, ... are shipped without fan controls. Check ... ... amperage on the fan motor(s ... ... . Verify the fan rotation direction. ... combination of ambient fan cycling and condenser ...
acpa4000 Spare Parts List
234-4206 CAP MTL PPR 45UF 10% 370vac ( compressor ... 0p4582 COMPRESSOR ROTARY 115/1/60 (PANASONIC style compressor ... 0M-6326A Condensate Pump EC -400 Little Giant (yk0501 below ... 0M-2470 Condenser Fan ( fan only 490-1045 Condenser Fan Box Sub Assy ( fan housing assy ... 870-3663 Evaporator Fan Box Assy ( fan only 490-1046 Evaporator Fan Box Sub Assy ( fan w/ housing assy ... 540-0088 Switch Thermal Overload Protector (for compressor pecker head
Where can I get support for APC and MGE Products?
AC Power ... Air Cooled Chillers ... InRoom Direct Expansion ... InRow Direct Expansion ... SmartSlot Expansion Chassis
Refrigerant charging table for a Uniflair Unit
... be short and direct as possible. ... proper refrigeration/ AC vibration clamps. ... return to the compressor . ... ) of the compressor to ensure that ... ... back to the compressor during shutdown Liquid lines must be sized to ensure sufficient refrigerant flow to the expansion device and to minimize pressure drop. ... 5. Start the compressor , and complete the charging process. ... to avoid compressor damage.
Why do I need refrigerant traps in my piping?
All Air Cooled Cooling Units ... both during the compressor on and off ... ... back to the compressor head, causing ... ... discharge of the compressor to the inlet ... ... lines will reduce compressor capacity and increase compressor work. ... returned to the compressor . ... muffler to my air conditioner ? ... close to the compressor as possible. A: Whenever a condenser is located above the compressor , an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.