Browse FAQs

NetBotz 755 supports up to 4 AP9520T/TH sensors

Published date: 11 August 2020

Issue:
NetBotz 755 manual incorrectly states 12 AP9520T/TH sensors supported

Product Line:
NetBotz

Environment:
NBWL0755

Cause:
An incorrect notation in the initial NetBotz 755 manual states that up to 12 AP9520T or AP9520TH A-link sensors are supported

Resolution:
The NetBotz MBWL0755 only supports up to 4 AP9520T or AP9520TH A-link sensors and the manual is incorrect. The manual will be changed but in the meantime, we've added this FAQ to hopefully limit confusion.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.