Temp threshold is to low or sensor is in wrong place
Resolution:
Check threshold and check placement of sensor. Threshold should be at least 3 degrees above max normal temp and sensor should be place in the front of the server rack at least 6 inches from front of the server with blanking panels in any gaps in the rack
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.