Details Returned from APC Devices via Advanced Device Crawlers
Published date:
21 December 2016
Issue:
Details Returned from APC Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for APC UPS systems assuming the APC DDF (Device Definition File) is installed on the NetBotz appliance and the APC UPS is SNMP enabled. Please note that not all information listed below is available on all APC models.
Resolution:
Battery Status
Time On Battery
Remaining Battery Capacity
Internal UPS Temperature
Battery Run Time Remaining
Battery Replace Indicator
Number of External Battery Packs
Number of Bad External Battery Packs
AC Input Phase
Utility Line Voltage
Maximum Utility Line Voltage Last Minute
Minimum Utility Line Voltage Last Minute
Input Frequency
Reason For Last Transfer to Battery Power
UPS Status
Output Phase
Output Voltage
Output Frequency
Current UPS Load - Rated Capacity
Current Load Draw on UPS
Nominal Output Voltage
Maximum Line Voltage Before Switching to Battery
Minimum Line Voltage Before Switching to Battery
Ambient Temperature Probe 1
Relative Humidity Probe 1
Ambient Temperature Probe 2
Relative Humidity Probe 2
Outlet Control
Overload Condition
Low Load Condition
Current Load
Outlet Control
MSP Outlet Control
Nominal Battery Voltage
Actual Battery Voltage
Battery Current
Total DC Current
DC Power Plant Model Number
Automatic Transfer Switch Model Number
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.