How do I reset the password on my AP5201/AP5202, AP5808/AP5816, or KVM0108A/KVM0116A Analog KVM product?
Published date:
16 June 2016
Issue
How do I reset the password on my AP5201/AP5202, AP5808/AP5816, or KVM0108A/KVM0116A Analog KVM product?
Product Line
Rack Accessories - KVM Switches
AP5201
AP5202
AP5808
AP5816
KVM0108A
KVM0116A
Environment
All serial numbers
All firmware versions (unless otherwise specified)
Small philips head screwdriver available
Cause
Lost or forgotten password
Resolution
Turn off the power to the Analog KVM Switch or Rack LCD with integrated KVM Switch.Open the top cover of Analog KVM Switch, and short the jumper marked "Restore Default Password". On the AP5808/AP5816, you need to open the rear section of the unit's cover and look for the jumper labeled J17. (The "rear section of the unit" refers to the portion of the AP5808 or AP5816 unit that houses the KVM Switch port connections and remains stationary in the rack when the Rack LCD portion of the unit slides in and out of the rack.)
With the jumper shorted, turn on power to the Analog KVM Switch or Integrated KVM unit, and wait until the LEDs stop blinking, then turn off the power.
Return the jumper to the open position, and replace the cover.
Turn the power back on for the device. The assigned usernames and passwords will all be cleared. Start the OSD with the default user name and password, which is blank for both username and password on AP5201/AP5202 and apc/apc for AP5808/AP5816 and KVM0108A/KVM0116A.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.