Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come with 2 years of factory hardware ... software support . The Data Center Expert appliance and ... active and complete software support in order to ... technical support and software upgrades. Software support contracts are required for the server which has a default 25 nodes (covered under base software support SKUs) as ... as each additional node license. ... not currently require support contracts .
Assigning global permission for newly created user is not allowed in vSphere vCenter 6.0 U 1b and 6.0 U 2a.
vCenter cluster having more than two nodes . vCenter Server is installed on ... ... your windows vCenter Server ... c:\ Program Files\MIT ... Copy the path (eg: c:\ Program Files\MIT\Kerberos\bin) Navigate to the registry path: HKEY_USERS\S- 1 -5-18\Environment ... Append the path copied before to the registry key's value data field eg: C:\ Program Files\*******; c:\ Program Files\MIT\Kerberos\bin ... Restart the Windows vCenter server
Data Center Expert | How do I upgrade my software version?
... for upgrading StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all versions) ... You must have a valid currently active software support contract to receive upgrade files. ... 1 ) Download the upgrade.zip ... 3) Login to the DCE Desktop Client, select the Updates Menu, and then select Apply Server Update. ... 5) Select Install Update to start upgrading the server . ... Upgrades usually take an hour or less to complete, but for certain upgrades it may take significantly longer depending on the number of devices and amount of historical data .
Data Center Expert | What virtualization environments are supported?
... supported for the Data Center Expert virtual appliance ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... The most recent information on supported virtualization ... EcoStruxure IT Help Center at: ... /360039289653- Data - Center -Expert- ... The Data Center Expert v7.x server is available as ... ... to five device nodes and one surveillance node . ... monitor additional device nodes and activate supported applications , or to migrate from a server hardware version to ... ... development of the Data Center Expert 7. ... The Data Center Expert virtual appliance ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... a DCE hardware server to a virtual server ? StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... As the data center is moving away from hardware servers and towards vitalization ... ... a virtual DCE server , there are ... 1 ) You must ... ... as the hardware server from which you ... ... if your previous server already has licensing ... base 25 device nodes and 1 surveillance node ) your will ... ... than the hardware server . ... on the new server . After verifying support contracts for the license keys and the server itself, technical ... license the virtual server .
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... SturuxureWare Data Center Expert requires a ... passcode and the Data Center Expert's MAC address ... StruxureWare Data Center Expert (DCE ... ... this, the server registers itself in ... ... notifies the DCE server that there is ... ... Afterwards, the server scans the unit to gather specific information about the alert ... 1 . In a ... ... add a new server , please click ... ... against an existing server please jump to ... ... AP9465 = StruxureWare Data Center Expert Basic ... ap9470 = StruxureWare Data Center Expert Standard
Data Center Expert | Getting Started
... started with a Data Center Expert Appliance. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... Deploying the Physical Data Center Expert Appliance ... Deploying the Virtual Data Center Expert Appliance ... restricted to 5 nodes . ... deploy the StruxureWare Data Center Expert Virtual Appliance ... ... of storage that Data Center Expert has within ... Getting Data Center Expert on the ... ... ensuring that your Data Center Expert (DCE ... ... Settings for StruxureWare Data Center Expert StruxureWare Data Center Expert Security Information (Protocols, ... Licensing and Software Support Data Center Expert requires continuous software support to receive upgrades ...
Creating an Aggregate Device within the KVM Access Software
... KVM Access Management Software and why it ... KVM Access Software (ships with ... ... wishing to consolidate nodes within their KVM Access Software All software versions ... (router, server , ethernet switch ... ... ports into a single Aggregate Device, ... counts as a single node , and only requires a single license. ... to that specific server without having to ... ... through the Access Software . When a ... down a specific server remotely they don't ... ... I have 300 node license but have 300 servers and 600 PDU ... devices, ( servers and PDU ports ...
PowerChute Network Shutdown shuts down an ESXi host in vSAN cluster before it has been moved to maintenance mode.
Data is located on ESXi Hosts H 1 & H2 ... 3 is a witness server , VM setting is "FTT = 1 "
LDAP/LDAPS Configuration with KVM1116P, KVM2116P, and KVM2132P Digital IP KVM Switches
... refer to the information below in order ... ... authorization through external programs . ... configure the LDAP server , you will ... 1 . Install the Windows Server Support Tools ... with Windows 2003 Server ... the Windows 2003 Support Tools. ... the Windows 2003 Support Tools: 1 . On your Windows Server CD, open the Support >Tools folder ... 1 . Open a ... 1 . Right click ... ... all Users > Programs > Administrative Tools ... 1 . Create a ... 1 . From the ... ... ID must be unique 1 . Open the ... 1 . Run ADSI Edit. (Installed as part of the Support Tools.) ... CN=Users node .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.