Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. All Product models , all serial ... ... FM Air/ Water /Glycol Model W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water Model ... coil C= Chilled Water Model C= Chilled Water ... In-Row Model ... Main C= Chilled Water Model W= Water Cooled ... G= Glycol Cooled BA=208 ... Model W= Water Cooled ... G= Glycol Cooled Model AFX 1 = 1 Bay
What is the RDU’s entering water temperature guidelines
... the RDU’s entering water temperature guidelines. All Product models , all serial ... Guidelines of water temperatures Entering Water Temperature of RDU ... 1 . What range of Entering Water Temperature should be ... ... there is a Water temperature inlet alarm ... If you water temperatures goes outside of requirements, capacity will be reduced, and you will see your OA's go into alarm based on their alarm set points. Typically if you chilled water source is starting to exceed its target set point, the chiller will alarm and begin to inform you of the problem as well.
What alarms can be automatically reset on a High Capacity Uniflair Unit
• Low Pressure • Circuit 1 Chilled Water High Temperature Threshold Exceeded
Video: How to set up load assist on a Uniflair unit.
Product line: Uniflair Gen 1 and Chilled Water Units.
What is the Difference between Glycol and Chilled water?
... are used interchangeably in some cases, as many sites run chilled glycol through their chillers instead of straight water because the water lines are ...
Video: How to change Humidify and Dehumidify set points in a Uniflair unit.
Product line: All Gen 1 Uniflairs with push button displays and all Chilled Water Uniflairs
Video: How to change the Temperature and Humidity Alarm thresholds on a Uniflair unit.
Product line: All Gen 1 Uniflairs with push button displays and all Chilled Water Uniflairs.
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof.
What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water . There should also be a consideration regarding humidity control.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.