Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... Galax VX or Galaxy VM. Galaxy VX, Galaxy VM ... To conform to California law SB 327 which requires the ender user to change the password when first logging into a network device. The display of the Galaxy VX and VM is part of the NMC and has been disabled. ... Use the console cable supplied with UPS ... Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... Assuming the UPS is connected to the customer network and is granted an DHCP IP address.