acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... operation while the PDU , UPS , or XR Battery Cabinet is ... 1 . Never work ... 2 . Perform the ... ... electricity to the PDU , UPS , or XR Battery Cabinet, ... ... working on the PDU , UPS , or XR Battery Cabinet. ... requires at least two persons to safely ... ... from the equipment frames ... system, install two 21 U side ... ... , there are two PSX/ PDU side panel installation ... a PSX or PDU . ... next to a PDU or UPS , then a PSX/ PDU side panel ( ... installed on the PDU or UPS .