Browse FAQs



What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
The NetShelter CX is constructed using Melamine Faced Chipboard (MFC). The NetShelter CX also uses a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate ( HPL ) on its top and MDF on its plinth base.
Video: How to remove an acsc100 front or rear panel
Issue: This video walks through on how to remove an acsc100 front or rear panel .
Video: PDU Outlet Panel Replacement on Symmetra LX & Symmetra RM UPS Systems
Cause The Outlet PDU panels installed on the rear panel of a Symmetra can be changed as the user's needs change.
How to remove door panels from a Network Air FM, ACFM, or ir40
... .Decrease the depth by removing the front doors, front fascia, kick panel , rear panels , and main circuit breaker.
Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
On APC UPS products this indicator is typically on the rear panel .
My Smart-UPS will not turn on.
It is usually located on the rear panel , next to the input power cord.
What are the basic troubleshooting steps for the APC AV H-Type power Conditioner ?
Choose the dimmer setting (see the sections on “Front and Rear Panels ” and “Setup the h10” in User Manual) ...
Video: What are the different sensitivity settings of a Smart-UPS?
... "SUA" Smart-UPS 1000va or larger have a sensitivity button on the rear panel of the UPS.
SmartConnect Device Registration when QR Label is Missing
If the label is not available on the top , front or rear panel of the UPS, manual registration is possible. 1. For SMC
Can the side doors or rear fan panels of the NetShelter CX/CX2 be secured with the NetBotz HID door handle? If not, is there a more secure option?
Issue: I customer is looking to make the side door more secure, thus making access to the rear fan panels more secure.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.