Browse FAQs



NetBotz camera may appear deactivated after upgrade to Botzware 4.6.1
nbwl0355 , nbwl0455 , nbrk0450 , nbrk0550, nbrk0570 , netbotz , bot, botzware camera grayed out,
Is StruxureWare DCE or NetBotz susceptible to the WannaCry vulnerability?
NetBotz nbwl0500, nbwl0420, nbwl0320, nbwl0355 , nbwl0455 , nbrk0450 , nbrk0550, nbrk0570
Status: "Drive not found" when configuring Netbotz External Storage using Advanced View application
Environment NetBotz v3 ( nbwl0355 , nbwl0356, nbwl0455 , nbwl0456, nbrk0450 , nbrk0550, nbrk0570 )
Are there any limits to the amount of users that can be added to a version 3 NetBotz appliance?
NetBotz ... NetBotz version 3 appliances ... NetBotz User names are limited without the advanced software pack ... Version 3 NetBotz appliances have a user name creation limit of 5 users. ... Note that the nbwn0005 is not compatible with the NetBotz nbwl0355 and the NetBotz nbrk0550 and nbrk0570 come with the advanced software pack pre-installed. The only appliances that can use the nbwn0005 are the nbrk0450 and nbwl0455 .
NetBotz | Scheduling Periodic Reports
NetBotz v3 Wall Appliance: 355/356 ( nbwl0355 /6) & 455/456 ( nbwl0455 /6) NetBotz v3 Rack Appliance: 450/451 ( nbrk0450 /1), 550 (nbrk0550), & 570 ( nbrk0570 ) ... NetBotz v2 and v3
NetBotz v3 | Serial connection issues
... a v3 NetBotz appliance. NetBotz v3 Wall ... /356 ( nbwl0355 /6) ... /456 ( nbwl0455 /6) NetBotz v3 Rack ... /451 ( nbrk0450 /1) ... & 570 ( nbrk0570 ) NetBotz v3 ( ... NetBotz version 3 appliances have integrated USB to serial adapters to allow connecting to the appliance using a USB-A to USB-B cable. ... After installing the correct driver, the NetBotz Appliance may still show as an unknown device within the device manager when using a USB 3.0 port on a Windows 7 system.
NetBotz | Do NetBotz support BACnet Integration?
Do NetBotz appliances support BACNET ... NetBotz 700 Series - NetBotz Rack Monitor 750 ... NetBotz 300-500 ... /356 ( nbwl0355 /6) ... /456 ( nbwl0455 /6) ... /451 ( nbrk0450 /1) ... & 570 ( nbrk0570 ) NetBotz 200 Series - NetBotz Rack Monitor 250 - NetBotz Rack Monitor 200 ... NetBotz 200, 300-500, & 700 Series (all versions) ... BACnet Integration is not currently supported by any Netbotz devices / appliances. NetBotz v3 (355, 450, 455, 550, & 570) & NetBotz 250 appliances do offer a Modbus output option.
Serial Terminal Connection Parameters for all NetBotz Appliances
... Parameters for all NetBotz Appliances NetBotz v3 Wall ... /356 ( nbwl0355 /6) ... /456 ( nbwl0455 /6) NetBotz v3 Rack ... /451 ( nbrk0450 /1) ... & 570 ( nbrk0570 ) ... for communications with NetBotz appliances. ... IP configuration on NetBotz appliances. ... Parameters for all NetBotz Appliances ... connecting to a Netbotz appliance or a NetBotz Central via a ... ... similar version 3 Netbotz , you must ... The NetBotz 200 uses a Null Modem cable and a baud rate of 9600. NOTE: When connecting to a NetBotz Central, you must use a NULL modem cable.
Downloading the MIB file for version 3 Netbotz.
Downloading the MIB file for version 3 Netbotz . ... NetBotz v3 Wall Appliance: 355/356 ( nbwl0355 /6) & 455/456 ( nbwl0455 /6) NetBotz v3 Rack Appliance: 450/451 ( nbrk0450 /1), 550 (nbrk0550), & 570 ( nbrk0570 ) ... NetBotz version 3 MIB ... Obtaining the NetBotz version 3 SNMP MIB file ... The SNMP MIB for NetBotz Appliances can be downloaded from the NetBotz Appliance itself by accessing the following URL: ... It should also be available on the product page for individual NetBotz appliances under the documentation tab.
NetBotz 300-500 Series | Password reset procedure
How do I reset the password on a 300-500 series NetBotz appliance. ... NetBotz v3 Wall Appliance: 355/356 ( nbwl0355 /6) & 455/456 ( nbwl0455 /6) NetBotz v3 Rack Appliance: 450/451 ( nbrk0450 /1), 550 (nbrk0550), & 570 ( nbrk0570 ) ... NetBotz 300-500 Series (all versions) ... On older Version 2 NetBotz 320, 420, and 500 appliances, the password alone can not be reset.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.