Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... RJ45 terminator ( included ) in the ... ... -0w05545a which includes qty 2 terminators ... ... been pre- installed for you in ... ... function in standalone installations . ... They have always included a terminator since ... ... Originally, AP86XX included a larger terminator ... ... also modifed to include a lower profile terminator pre- installed . ... serial numbers will include a pre- installed low profile terminator ... ... " port of one of the grouped ...