Technical FAQs

Ask a Question

Filter results

    Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
    APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
    Used Battery Disposal Options
    If you purchased an APC Replacement Battery Cartridge in the U ... return the old battery will be provided with the new Replacement Battery Cartridge .
    How do I recycle APC batteries in the US and Canada?
    Please find two options for recycling the old batteries below. They may be recycled locally using call2recycle or though our Replacement Battery Cartridge Recycling Program.
    Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
    In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
    Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
    Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
    How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
    To determine the correct Replacement Battery Cartridge to purchase for your APC UPS and to see other options available to you, use the
    Discontinuation of Replacement Battery Cartridge 44 (RBC44)
    Cause: APC by Schneider Electric announces the discontinuation of the Replacement Battery Cartridge 44 (RBC44
    What are the basic troubleshooting steps for the APC AV J-Type J25B / J35B Power Conditioner and Battery Backup?
    ... steps for the APC AV J- ... Power Conditioner and Battery Backup ? APC AV J- ... Power Conditioner and Battery Backup ... find the your APC AV J- ... The internal battery is not connected ... Connect the battery . ... connect to a Battery Backup outlet. ... is operating on battery power, while ... Battery Backup outlets may ... ... equipment from the Battery Backup outlets and ... The battery was recently discharged due to a power outage and has not fully recharged. Charge the battery cartridge for 16 hours. The battery has reached the end of its useful life. Replace the battery .
    Can I mix old and new batteries in a Smart-UPS?
    ... old and new batteries in a Smart ... ... either multiple internal battery cartridges and/or ... to add external batteries . ... old and new batteries within the same ... ... Lead Acid) batteries age, their ... ... Smart-UPS batteries are connected in parallel and all batteries are charged at ... Mixing batteries of different ages ... result in some batteries being under charged ... When replacing the batteries in a Smart ... , you should replace all battery modules (internal ... ... adding additional external battery packs to a ... you should first replace the existing batteries (internal and ... ... should not mix batteries with more than ...
    Why are the battery charge LEDs flashing on a Smart-UPS?
    Battery Charge LED Bar ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... ... the load or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ...
    Results 1 - 10 of 50