Resolution:
Yes, there are 2 power supplies in the unit for the condenser and evaporator fans. If 1 fails the other can supply 70% of the maximum power needed, so maximum fan capacity would be reduced approximately 30%. They are hot swappable as well; a user can replace the failed power supply from the front of the unit while the ACSC is still in operation. The evaporator fans are also hot swappable.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.