Browse FAQs



UPS Signalling Bundle for IBM AS/400 & IBMi (IBM Power Systems)
This document also reviews installation, supported APC UPS systems , system requirements, and set up. Important Configuration Information
Serial communications between Smart-UPS VTs, Galaxy 3500, and Symmetra PX with IBM AS/400, i Series
*Available UPS Signalling Options for IBM AS/ 400 & IBMi ( IBM Power Systems ) can be found in FAQ FA159551
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... with the g3500 to supply two dedicated simple signaling ports, such as for use with an AS/ 400 or an IBM iSeries, ...
PowerChute Network Shutdown compatibility with IBM AIX installed on LPAR
How to configure PowerChute Network Shutdown on IBM AIX which is set up on LPAR. ... IBM AIX 7.2 on LPAR. ... If UPS is Smart- UPS SMT, SMX, SRT Enable Power off the Hypervisor automatically after all LPAR are shut down ... Select Do not turn off the UPS ... The options are Turn off Outlet Group when: power failure last longer than or UPS runtime is less than. ... If the Smart- UPS is NOT a SMT, SMX, SRT Enable Power off the Hypervisor automatically after all LPAR are shut down ... Select Do not turn off the UPS
Did APC purchase the AirFlow Company?
American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... 2000 - American Power Conversion (NASDAQ ... ... today’s datacenters are power and heat. As the power density continues to ... Similar to power disruptions, temperature ... ... IT and telecommunications systems through the precise ... and humidity, system redundancy and the ... ... well as management systems used in a ... ... Its solutions also offer one of the ... ... patented Symmetra® Power Array(TM ... -phase uninterruptible power supply ( UPS ) manufacturer Silcon ... S and DC power system company Advance Power , as well ... ... their global datacenter power and cooling needs ...
Video: Why might my APC Back-UPS Product be beeping?
... operating on battery power - ... indicates that the UPS has transferred from ... The Battery Power Supplied outlets are now battery powered . ... indicates that the UPS has reached a ... The UPS can only operate ... ... much, the UPS will shutdown and ... ... shutdown, the UPS will sound this ... APC's UPS Selector ... indicates that the UPS has detected an ... ... determine if your UPS is capable of ... ... .) Disabling UPS audible alarm tones ... ... software, the UPS audible alarm tones ... ... operating on battery power ... equipment, the UPS will transfer to ... The UPS is trying to ... , and reliable power .
Do I need to use a 24VDC power adapter with the Isolated Extension Cable?
When attempting to connect a system running PowerChute in simple signaling through an Isolated ... 24VDC adapter to power the UPS End Unit of the IEC ...
Why would I need to use the 24VDC adapter when using the APC Isolated Extension Cable?
When attempting to connect a system running PowerChute plus in simple signaling through an Isolated ... 24VDC adapter to power the UPS End Unit of the ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.