Browse FAQs



Can StruxureWare Data Center Expert be configured to alert for NetBotz 3xx, 4xx, and 5xx devices?
Can StruxureWare Data Center Expert be configured ... StruxureWare Data Center Expert StruxureWare Data Center Expert monitoring NetBotz ... StruxureWare does not alert ... This was done to eliminate NetBotz Central as a single point of failure. ... The only alert StruxureWare DCE will alert for is if DCE itself loses communications with the NetBotz device (and only if the DCE server has a user with an associated e-mail that also has access to that NetBots appliance.) ... Please note that this is different than the NetBotz Rack Access AP9361, NetBotz 200 , or NetBotz 250 which are monitored using SNMP.
Data Center Expert | How do hardware and software support contracts work?
Cause: StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no
Is StruxureWare DCE or NetBotz susceptible to the WannaCry vulnerability?
Is StruxureWare DCE or NetBotz ... StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Operation (DCO) ... Network Management Card 1 ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ap9340, Netbotz 200 , NetBotz 250 ... ... Metered/Switched Rack PDUs (AP84XX ... ... find out if StruxureWare DCE or NetBotz ... More information on these platforms can be found on http://DCIMsupport.apc.com
StruxureWare Data Center Expert v7.4.2 is no longer available
Resolution You must have a valid support contract to receive the software update.
Data Center Operation | Video: Copying files from the StruxureWare Data Center Operation
1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
... ISX Manager or StruxureWare may not work ... ... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ap9340, NetBotz 200 ) ... Metered/Switched Rack PDUs (AP86XX ... ... ISX Manager takes one device's configuration file ... ... retrieve and push one from another device ... ... password using the information from the [ ... APC has a utility that sends one config file to many devices. ... If you have ISX Central or StruxureWare Data Center Expert, this should not be an issue.
Configuring rack access cards using both StruxureWare DCE and NetBotz Advanced View causes an exception
1 . Remove all the rack access cards from the NetBotz Advanced View and StruxureWare Data Center .
How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
1 ) Navigate to ... Installation directory for StruxureWare Data Center Expert. ( ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X. ...
What is the maximum number of rack access cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards ...
Video: Where can I download the StruxureWare Data Center Expert client software?
Resolution: 1 ) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.