Browse FAQs



PowerChute Network Shutdown reports "Available runtime has been exceeded".
... event actions are carried out even if it occurs on a single UPS in a Redundant or Parallel UPS configuration .
Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs
46934 Info IM internal memory for storing configuration settings is OK IO enclosure level ... Info RTC Time adjusted value Parallel UPS 1 2 02- ...
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... Smart- UPS VT & Galaxy 3500 Battery XR frames ... How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... This means that you shall connect UPS and XR in parallel by applying +24V on both connectors UPS j108 & XR j203, if you will EPO them both at same time. ... UPS can be configured in three other ways, concerning EPO. See UPS Installation manual for details.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Smart- UPS ... the use of Parallel Kit(srcpk001 ... ... A: The Parallel Kit allows you ... ... equally but if one fails (either ... , the other UPS will take over ... ... information of the UPS operation condition such ... ... addition to the 1 + 1 Parallel redundancy system, ... ... to take a UPS out of operation ... to bypass the UPS without taking their ... ... , isolating the UPS and connected equipment ... step-down transformers are used to convert a higher input voltage to a lower output voltage which might be more fitting for certain environments or system configurations .
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... about the Matrix UPS ? Matrix UPS ... of a Matrix UPS . ... the APC Matrix UPS . 1 . Matrix- UPS should be set ... ... to Matrix- UPS . ... , Matrix- UPS Input Select Tap ... ... Set Matrix- UPS EU (Electronics ... of Matrix- UPS IU (Isolation ... ... of Matrix- UPS or by its ... ... from EU's " batt com" input ... ... of Matrix- UPS IU to " ... ... current Matrix- UPS settings . ... to menu " UPS Tests" and ... Matrix- UPS Noises ... The Matrix- UPS will make certain ... 1 . Loud Hum ...
Default administrator authentication phrase used by PowerChute Network Shutdown to communicate with the Network Management Card
If you are using a Redundant Smart- UPS , Multiple Symmetra, or a Parallel UPS configuration , all of the NMC authentication phrases ...
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... to Smart- UPS drops or reboots ... Smart- UPS ... a Smart- UPS can be dropped ... 1 ) - A UPS with a weak ... ... Every Smart- UPS has a " ... ... failure which the UPS self test may ... ... result in unexpected UPS behavior including load drops and the UPS turning off: - Each UPS is limited in ... ... number of the UPS tells you the ... ... determine if your UPS is capable of ... please use our UPS Selector Tool at ... plugged into the UPS , but the ... . If the UPS and surge strip ... A single piece of equipment ...
How to set self test day and time on Symmetra UPS products
... time on Symmetra UPS products 1 ) A UPS load on command ... ... self test interval setting . ... the self test setting ... ) to main UPS menu Your UPS self test should ... ... , 100, 160 kVA the menu ... UPS -> UPS Configuration -> Other ... ... that anytime the UPS is commanded on ... ... outage causes your UPS to fully drain ... to when the UPS is turned back ... Also, if your UPS was turned off while in maintenance bypass for a repair, upon restart the self test counter would also be reset.
How to change the Input Voltage Select Jumper on a Symmetra Power Array
... the input voltage setting ; what is ... Before the UPS is started up ... : UPS must be completely ... 1 . Switch the ... ... front of the UPS . ... that feeds the UPS . 4. Remove all battery modules from the UPS . 5. Disconnect any extended run (XR) battery frames from the UPS . ... 1 . Refer to figure below. ... 2. Use a small, flat head screwdriver to position the input voltage jumper to the correct voltage setting . ... 3. Replace the voltage select access panel and continue with connecting the UPS to utility power.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.