Browse FAQs



What effect, if any, do the magnetic panels of the Vertical Exhaust Duct Kits have on high speed network cables?
Issue: The NetShelter SX Vertical Exhaust Duct Kits include magnetic panels.
Which NetShelter SX cabinet has a greater cable capacity, 750mm wide or 800mm wide?
For example; ar7580a is the high volume vertical cable manager used in ar3150 and ar3350, and also in ar3180g and ar3380g.
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
Environment: All 750mm wide NetShelter SX cabinets: ar7580a, AR7585, AR7588, ar8008blk, ar8016ablk; all serial numbers.
Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
Issue: A customer may want to install the AR7721, AR7722 or AR7723 into a wide NetShelter SX or SV.
Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
Issue: The ar8008blk and ar8016ablk are designed to install into the mounting rails of NetShelter SX 750mm wide cabinets.
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... Rack Expansion Bundle Kit Installation (Manual ... ... Rack Expansion Bundle Kit is a complete ... panel required to extend an existing Hot ... ... Rack Expansion Bundle Kit is a complete ... panel required to extend an existing Hot ... ... Cabinet, in case of an emergency ... ... Rack Expansion Bundle Kit . ... on each doorframe upright to remove the ... ... -mm) enclosure . ... Rack Expansion Bundle Kit next to a ... ... 1070-mm enclosures ... -mm) enclosures : ... doors of the enclosures before you install ... ... 1070-mm enclosures ... -mm) enclosures : ... doors of the enclosures before you install ...
Can the vertical cable trough from the rear of the front left hand rail of a NetShelter Networking cabinet be moved to the left hand side, or is there a version that installs onto the right hand rail?
... asking if the vertical cable trough can be ... NetShelter SX Networking cabinets. ... using the same vertical cable duct as the front ... The vertical cable trough that's installed ... The NetShelter Networking cabinets are designed to be used with side airflow duct kits , which is why the rails are much thinner. This provides maximum airflow when side airflow switches are installed with duct kits . ... Each NetShelter Networking cabinet ships with a set of Airflow Management Panels that are used to block any open areas above or below where a side airflow duct kit is installed.
Are 23" mounting rails available for NetShelter SX cabinets?
For customers who already own a 42U 750mm wide SX cabinet with 19" mounting rails (ar3150 or ar3350) we offer sku ar7510 ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.