Browse FAQs



NetBotz 450/550/570 | Physical Description
... Description of the NetBotz 450/550 ... NetBotz version 3 NetBotz v3 Rack ... ... third-party dry - contact sensors, and ... ... Third-party dry - contact state sensors require the NetBotz Dry Contact Cable (nbes0304) ... ... sensors require the NetBotz 0-5 V Sensor Cable (nbes0305) ... ... for connecting a NetBotz Rope Leak Sensor ... ... Used for cascading NetBotz sensor pods and ... ... CAT-5 cabling with straight- ... 15 Power LED Indicates ... The complete NetBotz 450/550/570 Installation and Configuration Manual can be found .
NetBotz 750 | Physical Description
... Description of the NetBotz 750 NetBotz version 5 NetBotz v5. ... ... CAT-5 cabling with straight- ... ... for connecting a NetBotz Leak Rope Sensor ... ... third-party dry - contact sensors, and ... Third-party, dry - contact state sensors require the NetBotz Dry Contact Cable (nbes0304), and third party, 0-5 V sensors require the NetBotz 0-5 V sensor cable (nbes0305). ... 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed. ... 15 Console Port Provides a serial connection to the appliance.
Wiring specifications for NetBotz Dry Contact Cables
Issue: Wiring specifications for NetBotz Dry Contact Cables
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
Sensor - 32 in nbes0311 NetBotz Dry Contact Cable (Requires BotzWare 4.5.0) nbes0304
NetBotz 355 | Physical Description
Third-party dry - contact state sensors require the NetBotz Dry Contact Cable (nbes0304).
NetBotz 455 | Physical Description
Third-party dry - contact state sensors require the NetBotz Dry Contact Cable (nbes0304).
NetBotz 250 | Physical Description
Third-party dry contact sensors require a Dry Contact Cable (nbes0304). 7 USB Port Used to connect USB devices to the appliance.
NetBotz 200 shows phantom sensors when multiple dry contact cables are connected.
It has been seen where 4 dry contacts may be listed while only 3 are connected.
DIN Connector Pin Outs For the Netbotz Appliances
... address this issue, NetBotz sells a standard dry contact cable that is our ... and two bare dry contact style wires on the other.
What are the pinouts of the RJ45 sensor connectors on a NetBotz appliance?
... address this issue, NetBotz sells a standard dry contact cable that is our ... and two bare dry contact style wires on the other.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.