Browse FAQs



Network Air FM unit spare parts list
... Network Air FM unit . Always Install ... Cable Lower ( Downflow ) ... /Water & Air LL ... CAT5 for EXP unit Duct Collar Downflow Filter Air 30% UF ... DF 5/ Unit 756 X 325 ... Filter Air 85% UF ... DF 5/ Unit 756 X 325 ... ... FIRE DETECTOR - DOWNFLOW ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... KW W/ AIR DEFLECTORS ... (for outdoor unit ) ... FM35-50 UNIT WIRING DOWNFLOW ... " Teflon FM units PowerView Label Air (NOME)
What are the factors that affect Battery Rated Service Life?
Frequency of discharges Number of discharges Maximum discharge rate Depth of discharges ... as well as discharging . Not many installations can maintain that ... This specification is for the internal temperature of the battery, and not for the ambient room temperature. Keep in mind if batteries are installed inside a cabinet, the internal temperature of the battery is usually 2 deg warmer than ambient air , and temperature at the top of the cabinet can be 10 F warmer, than at the bottom. ... – This is how often the battery charges and discharges . ... - The VRLA battery is specifically designed to be installed
Batteries discharged to a low voltage in a single phase Symmetra frame
... battery modules are discharged below 95 VDC ... ... bus voltage may discharge to a voltage ... ... battery modules are installed in a Symmetra ... ... the batteries left installed in the frame, they will discharge to a voltage ... ... and Symmetra RM units ship with caution ... customer not to install the battery modules ... ... to remove all discharged battery modules installed in the system ... ... equalize with the discharged battery modules and also become discharged . ... experience a deep discharge under 80vdc should ... due to possible internal battery cell damage ... If the discharged battery modules were ...
How to navigate through an Network Air FM unit display
... through an Network Air FM unit display. ... ACFM, Network Air , ir40. ... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... ... of the return air and the dew ... ... of the return air . ... (PCIOMs) installed in the user ... Installation ... of air filters installed in the Modules ... ... recommended for typical installations . Air When the unit is in dehumidification ... ... DX 60 Hz Installation ... and humidity probes installed must be supported ... ... flow switch is installed : ... condenser valve is installed . ... isolation valve is installed in the coolant ...
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package
How to Install a OROA or A LAC Valve as part of a Flooded Receiver Package. ... ACRD1XX, ACRD2XX, ACRP1XX, ACRD5XX, Uniflair DX, Network Air FM, InRoom DX. ... Install . ... The installation of the valve requires the proper alignment. ... D= Discharge line from the Compressor.
How to remove door panels from a Network Air FM, ACFM, or ir40
How to remove door panels from a Network Air FM, ACFM, or ir40. ... acfm200, acfm400, Network Air FM, ir40. ... Install . ... For safety, have at least two people lift and move them during removal or installation . ... Tilting the equipment more than a few inches from the vertical may cause internal damage. ... Removing and installing the side panels Remove side panels to access internal components or to join equipment. ... 3. Reverse this procedure to install the panels.
Uniflair Drain Line Connections
Install , Repair ... fitted in the unit . If the unit is fitted with ... ... . Connect the unit drainage tube to ... tube with an internal diameter of 1 ... : The installation must comply with ... ... trap inside the unit is full. Warning: The water discharged from the humidifier is at a very high temperature. ... 1. Connect the unit drainage tube to the humidifier collection tray. 2. Connect the humidifier drainage tube to the building drains using a rubber or plastic tube, which is resistant to high temperatures minimum (212°F) with an internal diameter of 1.26”.
Why do I need refrigerant traps in my piping?
... Air Cooled Cooling Units ... A: A discharge line trap plays ... ... entrained in the discharge gas and to ... ... are utilized in discharge risers and at ... ... pipe diameter for discharge risers. ... advised to always install a single trap ... ... or oversize my discharge line since I ... A: Discharge gas lines ( ... flow from the discharge of the compressor ... Undersizing discharge lines will reduce ... Over sizing discharge lines increases the ... Undersized discharge lines reduce system ... ... Oil movement in discharge lines is further ... ... for a typical Discharge Line installation ... to add a discharge muffler to my ...
EcoBreeze Variable Speed Drive Technical Spec’s
Supply Internal supply for logic ... Internal supply for reference ... ... -segment display units for CANopen bus ... ... 100 Hz Display unit 0.1 ... immunity test conforming to IEC 61000-4-4 level 4 Electrostatic discharge immunity test conforming to IEC 61000-4-2 level 3 ... Ambient air for storage -25...70 °C Ambient air for operation -10...50 °C without derating with protective cover on top of the drive -10...60 °C with derating factor without protective cover on top of the drive
What are the operational conditions for an InRoom (Stulz) Unit
... (Stulz) Unit . Install ... precision air conditioning units operate within the ... ... between the cooling unit and the air ... ... and the cooling unit : 5 m ... below the cooling unit Return air conditions for evaporator capacity (DX): 24°C (75°F) 50% R. H. Return air conditions for cooling capacity (CW): 24°C (75°F) 50% R.H. ... Downflow units with an external static pressure: 20 Pa (0.08 in w g)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.