Browse FAQs



Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
Each of these areas has slots to support up to two of the cable side channels . (4 cable side channels total)
Can ar8008blk or ar8016ablk be used in the NetShelter Networking cabinets?
In the Networking cabinets horizontal cable managers can be used to connect the side channels from front to rear.
Can NetShelter horizontal cable managers be mounted back-to-back?
Cause: In some installations it may be advantageous to mount the horizontal cable managers on both sides of the mounting rail.
Can cable management arms such as AR8129 be used in NetShelter CX cabinets?
A customer wants to install the cable management arm into a NetShelter CX cabinet. ... Cable management arms can be used but must be confined to specific U-spaces so they don’t interfere with the fan modules. Also, if the cable entry channel is being used care should be taken when installing AR8129 in the lower U-spaces. • In the ar4018a or ar4018ia the AR8129 can only be mounted in U-spaces 1 through 7, and 12 through 18 .
Can APC Cable Managers be installed into any other manufacturers' cabinets?
... of cabinets and cable management from different ... ... NetShelter Vertical and Horizontal Cable Management ... to install NetShelter cable management products into ... Rackmount horizontal cable managers are EIA ... Vertical cable managers that connect ... Vertical cable managers that connect to square cage nut holes in a NetShelter SX cabinet will also install into the square cage nut holes in other manufacturer's cabinet. ... Vertical cable managers that connect to the teardrop shaped mounting holes of a NetShelter SX 0U Accessory Channel may to be compatible with any other manufacturers' cabinets, although we do not track compatibility with other manufacturers.
ACSC1XX Spare Parts List
CABLE ASSY RELATIVE HUMIDITY ... CABLE ASSY RELATIVE HUMIDITY ... CABLE ASSY Temperature Humidity ... CABLE ASSY Temperature Sensor CABLE ASSY TEMPERATURE SENSORS CABLE ASSY TEMPERATURE SENSORS ... OD ( 18 " long PVC ... OD ( 18 " long PVC ... ... (for power cable at the bottom ... LATCH FLUSH SLAM W/ TUMBLER #333 (for side door panels) ... Leak Sensor - 20 ft (6.1 m) (ships with orange sensor [AP9326] & black cat5e cable ) ... Thermistor/Probe EMU Cable ASSY - Spare Part (13FT PURPLE) ... WIRE CLIP - BLACK AP9335TH (holds sensor cables )
Why does my local mouse (the mouse on the server I am connecting from) not synchronize with my remote mouse (the mouse on the server I'm connecting to) when connected through the APC IP KVM product?
If the Index side navigation bar is shown in tree view, click the plus symbol (+) next to Peripherals to display the submenu items. ... Certain Sun/Linux Varieties adjustment via Terminal Session ... Length and type of Ethernet cable being used between the KVM and the server.
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... or by its side . 5. Hook Anderson connector from SmartCell battery pack to EU slot, then add SmartCell communications cable . ... : Battery communication cable must go from EU's "batt com" input to the "output" marking of first SmartCell. ... The UPS withstands EM fields of 10 V/m over a frequency range of 10 kHZ to 150 kHZ, and 80% at 1 kHZ at 10 V/m over a frequency of 150 kHZ to 1 GHZ for both vertical and horizontal polarization. The
Network Air FM unit spare parts list
25 Pin Cable Lower (Downflow) ... 25 Pin Cable Lower (Upflow) ... 25 Pin Cable Upper ... Door Assy LH SIDE FM UF BLACK ... FLOORSTAND 18 " FM35-50 KW W/AIR DEFLECTORS ... Rope Water Detector Assembly (0w1586 cable only) ... SEISMIC FLOORSTAND, 18 " FM 35-50 KW W/AIR DEFLECTORS ... VFD COM E BOX CABLE ASSY FM35-50
DAC, Cancoil Installation Manual
... . Controls and Adjustment ……… ... ... for ease of adjustment . ... clearance on all sides of the condenser ... Horizontal pipe runs should ... Horizontal pipe runs should ... Use a good vacuum pump designed specifically for this duty.Connect the vacuum pump to both the high side and the low side of the system with 1/4” minimum ID Copper tubing. ... Section 6. Controls and Adjustment ... The following paragraphs describe the function and adjustment of the various components.Cancoil ... No further seasonal adjustment is required after this.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.