Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
... hardware warranty and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come with 2 years of factory hardware ... software support . The Data Center Expert appliance and ... active and complete software support in order to ... technical support and software upgrades. Software support contracts are required for the server which has a default 25 nodes (covered under base software support SKUs) as ... as each additional node license. ... not currently require support contracts .
Creating an Aggregate Device within the KVM Access Software
... within the KVM Access Management Software and why it ... KVM Access Software (ships with ... ... wishing to consolidate nodes within their KVM Access Software All software versions ... (router, server , ethernet switch ... managed through KVM Access is capable of being accessed through several devices ... ... as a single node , and only ... ... to that specific server without having to ... ... management through the Access Software . When a ... down a specific server remotely they don't ... they can just access that specific aggregate ...
Data Center Operation | Upgrade Process
... and upgrading StruxureWare Data Center Operation . StruxureWare Data Center Operation (DCO) StruxureWare Data Center Operation (all versions ... ... Upgrade files for Data Center Operation are now provided ... EcoStruxure IT Help Center . ... Creating a Help Center Account & Associating your Server (Online/ ... Upgrading the Data Center Operation Server ... within the Help Center ... EcoStruxure IT Help Center Account & Associating your Server ... Log into your Data Center Operation (DCO) ... ... EcoStruxure IT Help Center site, proceed ... 3 ) Log into ... ... EcoStruxure IT Help Center - Offline Product ... ... EcoStruxure IT Help Center site at: ...
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... a DCE hardware server to a virtual server ? StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... As the data center is moving away from hardware servers and towards vitalization ... ... a virtual DCE server , there are ... ... as the hardware server from which you ... 3 ) Register the ... if your previous server already has licensing ... base 25 device nodes and 1 surveillance node ) your will ... ... do not have access to your company's ... ... than the hardware server . ... on the new server .
IPMI Overview
... Version 2 and 3 appliances ... devices (mostly servers ). ... interface into their server’s hardware at a ... Implemented on server’s baseboard management controller ... ... status, environmental info , etc internally ... ... into third party software applications (NetBotz) ... NetBotz Support of IPMI ... IPMI-enabled servers and network equipment ... Midrange & enterprise servers will have multiple of each type of sensor ... IPMI is supported on the NetBotz 500 , 420, 320 with a valid Premium Software Module key installed IPMI is supported on the NetBotz 450, 455, 550, and 570 units with a 5 node monitoring pack (nbwn0006) installed.
APC Security Advisory - InfraStruxure Central 5.0 Java Runtime Environment
... processing of XML Data . ... processing of XML data may allow unauthorized access to certain URL ... ... with processing XML data may allow an untrusted applet or application that is downloaded ... a website unauthorized access to certain URL ... ... of malicious XML data InfraStruXure Central Server ... uploading of XML data , the data must adhere to ... ... the InfraStruXure Central Server using the next ... ... untrusted applet or application to elevate its ... ... or execute local applications that are accessible to the user ... ... Environment Scripting Language Support . [ 3 ] ... to scripting language support may allow an untrusted applet or application to elevate its ...
LDAP/LDAPS Configuration with KVM1116P, KVM2116P, and KVM2132P Digital IP KVM Switches
... refer to the information below in order ... ... authorization through external programs . ... configure the LDAP server , you will ... ... Install the Windows Server Support Tools 3 . Extend and ... ... with Windows 2003 Server ... the Windows 2003 Support Tools. ... the Windows 2003 Support Tools: ... On your Windows Server CD, open the Support >Tools folder ... 3 . Follow the ... 3 . Open the ... ... all Users > Programs > Administrative Tools ... 3 . In the ... 3 . Edit the ... 3 . Select New ... 3 . In the ... ... part of the Support Tools.) ... CN=Users node .
Data Center Expert | Discovering a NetBotz 300-500 Series Appliance
... 400, or 500 series appliance into StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... NetBotz v 3 Wall Appliance: ... NetBotz v 3 Rack Appliance: ... StruxureWare Data Center Expert (all ... ... NetBotz 300- 500 Series Appliance ( ... ... NetBotz 300- 500 Series Appliance 3 ) Select the ... ... NetBotz 300- 500 & 700 series ... ... Appliance 300- 500 Series Device Discovery ... ... NetBotz 300- 500 Series Discovery ... ) Under Additional Information select Troubleshoot Network ... 3 ) Under Function ... Appliance under Target Host and click Submit ... ... the Advanced View Application . Instructions for ...
Why does StruxureWare Data Center Expert not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert ... StruxureWare Central / Data Center Expert all versions ... SturuxureWare Data Center Expert requires a ... passcode and the Data Center Expert's MAC address ... 3 . If you ... ... add a new server , please click ... ... against an existing server please jump to ... ... AP9465 = StruxureWare Data Center Expert Basic ... ap9470 = StruxureWare Data Center Expert Standard ... AP9475 = StruxureWare Data Center Expert Enterprise ... AP94VMACT = StruxureWare Data Center Expert Virtual Machine ... SFDCOBASE = StruxureWare Data Center Operation ... a hardware DCE server and in help ... a VM or Data Center Operation .
Data Center Expert | How do I upgrade my appliance version?
... for upgrading StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... ... valid currently active software support contract to recieve upgrade ... 2) Login to the DCE Desktop Client, select the Updates Menu, and then select Apply Server Update. ... 3 ) Select Import and navigate to the extracted upgrade file. ... 4) Select Install Update to start upgrading the server . ... Upgrades usually take an hour or less to complete, but for certain upgrades it may take significantly longer depending on the number of devices and amount of historical data .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.