Browse FAQs



InRow RC Standard and Optional Features
Data Center Cooling ... 1-The Standard Features of the InRow Rc Coolling Unit are as follow: ... Chilled Water Flow Meter ... Pipe Adapters Top or Bottom Piping ... Power Trough (Overhead power distribution between racks) Data Partion Trough (Allows removal of RC unit without disrupting cabling)
DAC, Cancoil Installation Manual
... 2. Refrigeration Piping ……… ... At delivery , inspect the ... ... this on the delivery receipt and file ... ... is found after delivery , immediately place ... ... provided in the unit . DO ... SECTION OF THE UNIT . ... use the refrigerant piping as a lift ... Unit Placement and Mounting ... unit should be securely ... ... clearance around the unit for proper servicing ... ... 2. Refrigeration Piping ... refrigeration hookups and piping should be done ... Piping must be kept ... ... oxidation inside the piping , purge the ... ... EQUIVALENT FEET OF PIPE ; allowances for ... Horizontal pipe runs should be ... Horizontal pipe runs should be ...
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification ... ) M= Main ... W= Water Cooled ... F= Water Cooled ... D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled Circuit coil Circuit coil Circuit coil C= Chilled Water C= Chilled Water M= Main C= Chilled Water M= Main A= Air ... ... W= Water Cooled ... G= Glycol Cooled BA=208 ... ... W= Water Cooled ... G= Glycol Cooled 12 (2 Bay ... ... W= Water Cooled ... G= Glycol Cooled
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
... won't install on top of the InRow cooling unit . ... NetShelter, InRow Cooling , Row Power Distribution ... the 300 mm chilled water cooling units so there's nowhere ... A NetShelter trough such as ar8580 or AR8561 may also be used to span the cooling unit but they can not be attached directly to them. NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof. ... The mounting tabs on the bottom of the bottom of the 300 mm wide trough may be bent out of the way if there are no mounting holes.
Network Air FM unit spare parts list
... CAT5 for EXP unit ... DF 5/ Unit 756 X 325 ... .7 X 12 .8 X ... ... DF 5/ Unit 756 X 325 ... .7 X 12 .8 X ... FLOORSTAND 12 " FM35- ... ... H/E PIPING ... H/E PIPING ... (for outdoor unit ) KIT FM35-50 UNIT WIRING DOWNFLOW ... Loss of mains board ( Mains Board) ... Main Controller Board (NOME Board) ... O-RING 1 3/8" Teflon FM units ... P66 Controller Single Circuit (dual circuit )P66-AAB-10 ... SEISMIC FLOORSTAND, 12 " FM 35-50 KW W/AIR DEFLECTORS
Uniflair Manual Start Up and Shut Down (PCO1)
... Start Up the Unit ... . Unlock the main switch. ... all of the circuit breakers on the ... ... and all system pipes have been bled ... 7. For internal pipe , it is necessary to remove the frontal security metal sheet. ... If an alarm is indicated, consult the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual. Turn Off the Unit 1. On the first user interface screen, press the UP or DOWN buttons until the SWITCH OFF UNIT screen appears. ... For additional information, see the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.
High Supply Temp Shutdown Installation on a NetworkAIR FM
Data Center Cooling ... , causing the unit to become idle ... ... located near the bottom on the left ... ... . From the main screen of the ... ... conditions of the circuit to either NO ... ... state of the circuit is at that ... ... would like the unit to do when ... ... . From the main screen of the ... ... field to System MAIN MODULE HIGH SUPPLY ... ... state of the circuit is at that ... 5. From the main screen of the display use this path: Setup >> System >> Alarms >> Temp Thrshlds ... Set the low threshold very low and the high above the cooling Setpoint plus the deadband and a exaggerated factor.
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... PEX (FOR PIPING - Compression coupling ... -0989 ADPTR PIPE 3" ENGL ... connecting to metric pipe ... ASSY ACRP CW MAIN CTRL w0w4760 CABLE ... ... CONTACTORs, & CIRCUIT BREAKERs ... CONTACTORs, & CIRCUIT BREAKERs ... Part w0w3107 Cable Main Power 208/ ... ... Part w0w3128 Cable Main Power 480v For ... ... Part w0w3127 Cable Main Power acrp5xx ASSY ... 2 0w3125 Cable Main Power acrp5xx ASSY ... ... w0w3116 CDU Metric Pipe Connection Kit acac20012 Circuit Board For Compact ... Circuit Board For Compact ... Circuit Breaker 2P ... ... 272 417 r0357 Circuit Breaker 2P ... ... 272 317 r0357 Circuit Breaker 3P ...
Refrigerant charging table for a Uniflair Unit
... for a Uniflair Unit . ... -cooled DX units must be connected ... ... • All refrigerant piping is type L ... ... refrigerant lines/ chilled water piping are free from ... ... • All refrigerant piping joints must be ... ... • All refrigerant pipes are installed with ... Isolate piping from structural surfaces ... ... length of a pipe run. ... the diameter of pipe : • For pipes running in a ... direction, select pipe size from the ... ... below to determine pipe diameter for vertical pipes . ... below to determine pipe diameter for horizontal pipes . Refrigeration Circuits ... maintaining the refrigeration circuit must only be ...
How to navigate through an Network Air FM unit display
... Network Air FM unit display. Path: Main > Setup > ... Mains In. Indicates the primary operating voltage required ... ... MultiCool® ( chilled water) and ... ... , then the cooling setpoint is used ... ... relays to the Main Module. ... avoid over- cooling while dehumidifying. When the unit is in dehumidification ... Path: Main > Setup > ... ... the modes ( cooling , reheat, ... ... communication with the Main Module of a ... ... communication with the Main Module is lost ... Path: Main > Setup > ... ... address of the Main Module on the ... Path: Main > Setup > ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.