Browse FAQs



APC Schneider Cooling Unit Identification
105= 105f 115= 115F DC=230/ 1 /60
What is the input voltage required for the InRow ACRD?
The InRow ACRD unit uses a single phase 208v/60hz input in NAM and a 230v / 50hz input in the rest of the ...
What is the input voltage required for the InRow acrd100/200? Is a power cord supplied with the unit?
The InRow RD unit uses a single phase 208v/60hz input in NAM and a 230v / 50hz input in the rest of the ...
Why is the UPS thermal dissipation rating calculated using efficiency data different from the value specified on www.apc.com?
The value calculated using efficiency data or the Efficiency Comparison Calculator is based on nominal environmental conditions (25C, 230v 50hz input), in green mode with a fully charged battery. ... Calculated values are typical for nominal conditions, and the ones specified on the website apply for worst-case scenarios.
Why do I get a false Site Wiring Fault Message on a international 230v Smart-UPS?
... UPS “RM2U” models (su700/1000/1400rmi2u) were introduced, one of the new features was the ability of the ...
Information on Online and On Battery operation of 3:1 Symmetra UPS systems
The output voltage can be set 220 / 230 / 240 VAC. The output frequency can also be set to either 50hz or 60hz.
Symmetra RM running on battery with good Input Voltage
This document describes one possible cause for a Symmetra RM running on battery power when adequate input power is available. ... One setting is the Output Frequency which is under the SETUP option in the Symmetra RM's PowerView. ... This setting can be changed to 50hz +/- 3hz, Full Range Tracking, or 60hz +/-3hz. ... However, if the UPS is configured for 50hz +/- 3hz, then the UPS will subsequently run on battery power due to either insufficient Voltage or Frequency.
What are the operational conditions for an InRoom (Stulz) Unit
208- 230v / 3ph / 60 Hz ... Frequency:60 Hz +/- 1 %
ACSC1XX Spare Parts List
1 1 1 1 1 ... -230/ 1 /60 ( ... ... -240/ 1 /50 ( ... ... -230/ 1 /60, ... 1 ... -240/ 1 /50 SC ... 1 1 1 ... , SC, 50hz - SPARE PART 1 1 1 1 ... WASHABLE IR SERIES 1 /2" ... FITTING 1 /8" ... FITTING 1 /8" ... 1 ... BULKHEAD MOUNT ( single float) 1 1 1 GROMMET RUBBER 1 1 /2"ID X 1 3/4"GD X 1 /8" ... 1


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.