Browse FAQs



Galaxy VM Seismic Certification and Anchoring Requirements.
Galaxy VM Seismic Certification ... Galaxy VM ... for documentation regarding Galaxy VM Seismic Certification ... ... the layout or construction of the floor ... Galaxy VM Product Home ... ... -supply- ups -/data ... -phase- ups / galaxy -vm/ N -ecbzda Galaxy VM- 2012 ... Galaxy VM OSHPD pre ... ... -SA- Galaxy VM Typical Seismic ... ... 9GN8T9_R 1 _EN/ Galaxy VM Installation Manual: ... Galaxy VM Seismic Anchoring Document: BYSN-9GN8T9_R 1 _EN Galaxy VM Seismic Certification Document: COCR-9X4HHB_R0_EN
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... ) circuit to Galaxy VX ? Galaxy VX ... ) circuit to Galaxy VX ? ... A35JB8_R 1 _EN. ... When the UPS is EPO'd, ... There is also an option in the UPS Tuner ( ... software) to have the UPS go to static bypass on EPO (default setting is no). ... Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... , 8, N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... One is down ( ... ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Where do I find an Operation Manual for Galaxy VX Series UPS?
Issue: Operation Manual for Galaxy VX Series
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
The instructions to power down the UPS are available on the display. This procedure is for a single UPS without an external bypass panel.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
This procedure is for a single UPS without an external bypass panel.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Issue: How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.