Browse FAQs



DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Air Cooled Condenser Installation and Operating Instructions DAC Air Cooled Condensers For information ... Cancoil air-cooled condensers have been ... ... equipment, proper installation and set- ... ... be used if air-cooled quipment is located ... Installation Date __ ... ... properly sized and installed to insure oil ... ... risers should be installed with a trap ... Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, ... are shipped without fan controls. Check ... ... high affinity for water . ... amperage on the fan motor(s ...
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... InRow Chilled Water ... Installation Services ... Outdoor Enclosures ... Software Installation ... Uniflair Chilled Water
APC Schneider Cooling Unit Identification
... FM Air/ Water /Glycol ... Expansion A= Air Cooled E= Air Cooled W= Water Cooled F= Water Cooled D= Water Cooled ... W= Hot Water ... C= Chilled Water ... C= Chilled Water ... C= Chilled Water ... Main A= Air Cooled W= Water Cooled ... ) A= Air Cooled W= Water Cooled ... ) A= Air Cooled W= Water Cooled ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... W= Water Cooled F= Water Cooled w/ ...
Refrigerant charging table for a Uniflair Unit
Install . Air-cooled DX units must ... to a remote outdoor condenser. ... Systems with remote outdoor condensers must have ... Install all refrigerant lines in accordance with applicable industry guidelines as well as local and national codes and regulations. ... • All refrigerant lines/chilled water piping are free from debris. ... • All refrigerant pipes are installed with proper supports and approved refrigerant line clamps. ... When brazing field- installed copper refrigeration lines, use a nitrogen purge to minimize ... Install a ball valve before the micron gauge to prevent damage to the micron gauge during charging.
What are the operational conditions for an InRoom (Stulz) Unit
Install Outdoor ambient conditions: ... Chilled water -/cooling water pipes: Maximum water head pressure: 10 bar (145 psi) Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) ... Entering water temperature (EWT) for CW coil: 7°C (44.6°F) Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Chilled water medium (CW): 0% Glycol
Carrier 30ra010-055 AquaSnap® Air-Cooled Chillers with ComfortLink™ Controls 50/60 Hz
carrier, chiller operations, install , start up and troubleshooting, aqua snap
How does a chilled water actuator work on an acrc301h to control dew point after a power loss?
How does a chilled water actuator work on an acrc301h to control dew point after a power loss? ... Install , Repair. ... Upon restart, the fans start first to allow the sensors some time to recognize the air temperature and humidity as well as the fluid temperatures.
What are the requirements for the acsc100 condenser unit
assuming fans at 100% ... 100% condenser fan speed ... head pressure by modulating the speed of the condenser fans . When the inlet temperature is too low the fans can not slow down enough and then the unit will not control the temperature in the room properly. ... Up to 0.25” (63 kPa) of additional static pressure beyond the standard duct kit installation can be tolerated with only a small impact on the condenser performance. ... You may need a booster or compensation fan maybe needed in many circumstances to prevent a significant reduction in performance.
How to set points and sensor offsets on a Uniflair High Capacity unit with Touch Screen Display
Install . ... • Circuit Entering Chilled Water Temperature Sensor Offset: - ... • Circuit Leaving Chilled Water Temperature Sensor Offset: ... Outdoor Temperature Sensor Offset: Delta ... • Hot Water (Reheat) Temperature Sensor Offset: Delta
Network Air FM unit spare parts list
Install ... 875-4183 Glycol/ Water LL ... 875-4182 Glycol/ Water & Air LL ... HEAT EXCHANGER - FM NAM 35KW WATER , R22 ... HEAT EXCHANGER - FM NAM 40kw WATER , R22 ... HEAT EXCHANGER - FM NAM 50kw WATER , R22 ... Indoor Receiver Relief Valve 425psig 3/8 MPT X 1/2 FLARE (for outdoor unit) ... Rope Water Detector Assembly (0w1586 cable only) ... Spot Water Detector (Assy. ... Water Flow Switch Assy


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.