Browse FAQs



Symmetra LX Spare Parts List
... parts for the APC Symmetra LX UPS system? Symmetra LX ... for servicing a Symmetra LX UPS. ... /240 VAC Symmetra LX systems ( Symmetra system part numbers ... Symmetra LX 4 kVA Power ... , 200v/ 208v - SYPM4KP Battery Modules APC Symmetra LX Battery Module - SYBT5 APC Symmetra LX Battery Module with flame ... APC Symmetra LX Intelligence Module - ... Symmetra LX Four-Post ... Symmetra LX / Symmetra RM Two- ... Symmetra LX frame electronics module – 200v/ 208v - SYAFSU13 Symmetra LX Input/Output ... – 200v/ 208v - SYAFSU14
Stacking limitations for single phase Symmetra and Matrix products
APC offers Symmetra LX Tower systems with integrated XR battery cabinets (ex. SYA16K16PXR) which require no assembly.
How do I address external battery frames connected to a Symmetra LX system that features an integrated XR cabinet?
Because of the integrated XR frame , addressing may not be intuitive. This document describes the correct addressing scheme to ensure proper operation.
Mounting the Symmetra LX in a 2 post rack
... 1) SYOPT12 must be purchased and used for each Symmetra LX mainframe or extended run ( XR ) battery frame that is to be ...
Converting Symmetra LX to and from rackmount and tower configuration
APCs recommendation is that an APC certified field service technician assists with this, as the frame must be carefully tipped to remove the casters ...
Video: How do I properly reset a Symmetra XR Frame Communications Card (SYXRCC or SYAFSU16)?
Symmetra Power Array Symmetra RM Symmetra LX The XR frame shows a fault ... related to the XR frame . ... card on the Symmetra Extended Run Frame . ... back of the Symmetra Extended Run Battery Frame and wait for ... 4) Reconnect the communication cable(s) in the back of the card and acknowledge the return of the green status light within 60 seconds the UPS will re recognize the additional batteries and adjust the runtime value accordingly to include the batteries located in the Extended Run Frame . The following video demonstrates the procedure of reseating and installing the Symmetra XR Communications Card:
Symmetra LX Battery Module Information Missing within v6.X.X Network Management Card Firmware Web Interface
... installed in a Symmetra LX UPS may notice ... For this specific issue, this relates specifically to the last battery installed within a Symmetra LX system, including any batteries located in any Extended Run ( XR ) frames beginning with model number prefix SYBFXXXX. ... Symmetra LX UPS and Extended Run Battery Frames. ... http://www. apc .com/tools/download/index.cfm ... The user can review the missing information via the PowerView LCD menu on the front of the UPS or at the battery module itself via the serial number sticker.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.