Browse FAQs



E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
Issue The XR frame of a single phase Symmetra displays E 3 ; The mainframe indicates an XR Frame Fault.
Symmetra LX Spare Parts List
... parts for the APC Symmetra LX UPS system ... Symmetra LX ... for servicing a Symmetra LX UPS. ... Spare parts for 208 /240 VAC Symmetra LX systems ( Symmetra system part numbers ... Symmetra LX 4 kVA ... Battery Modules APC Symmetra LX Battery Module - SYBT5 APC Symmetra LX Battery Module with flame ... APC Symmetra LX Intelligence Module ... Symmetra LX Four- ... Symmetra LX/ Symmetra RM Two- ... Symmetra LX frame electronics module – ... Symmetra LX Input/ ... Symmetra LX Communications Card ... Symmetra LX 13 U ... Symmetra LX 19 U ... Symmetra LX 32 U ... Symmetra LX Castor kit ...
How to change the Input Voltage Select Jumper on a Symmetra Power Array
... environment of my Symmetra Power Array and ... Symmetra Power Array ... The jumper must be set to match the user's input voltage, either 208 or 240 VAC. ... 3 . Open and lockout the circuit breaker for the circuit that feeds the UPS. 4. Remove all battery modules from the UPS. 5. Disconnect any extended run ( XR ) battery frames from the UPS. ... Remove the screw that secures the voltage select access panel to the frame . ... 3 . Replace the voltage select access panel and continue with connecting the UPS to utility power.
Video: How do I properly reset a Symmetra XR Frame Communications Card (SYXRCC or SYAFSU16)?
Symmetra Power Array Symmetra RM Symmetra LX The XR frame shows a fault ... related to the XR frame . ... card on the Symmetra Extended Run Frame . ... back of the Symmetra Extended Run Battery Frame and wait for ... 3 ) Reseat the ... ... recognize the additional batteries and adjust the ... to include the batteries located in the Extended Run Frame . The following video demonstrates the procedure of reseating and installing the Symmetra XR Communications Card:
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
What are the lengths of the DC cables that are attached to single phase Symmetra extended run ( XR ) frames? ... Single Phase Symmetra XR Frames ... These products are designed to be able to reach each other if position in the same area . This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example. ... The following table outlines the cable lengths of the DC cable provided with each of the single-phase Symmetra Extended Run cabinets. XR Type ... SYARMXR3 Fixed 3 .5ft (1.0m)
How do I address external battery frames connected to a Symmetra LX system that features an integrated XR cabinet?
How do I address external battery frames connected to a Symmetra LX system that features an integrated extended run ( XR ) cabinet? ... Symmetra LX ... Symmetra LX with built-in XR frame only (for example, SYA16K16PXR or SYAF16KXR9T) ... Because of the integrated XR frame , addressing may not be intuitive. ... The user must set the first external extended runtime cabinet to " 3 " vs the normal "2" setting. The built-in battery cabinet acts as frame "2" even though it is integrated into the mainframe.
Converting Symmetra LX to and from rackmount and tower configuration
Symmetra LX APC by Schneider Electric ... ... to modify the Symmetra . ... when converting from rackmount to tower form ... ... : SYAOPT1 - Symmetra LX rack mount ... contact APC Customer Support ... to convert a Symmetra LX tower to ... APCs recommendation is that an APC certified field service ... , as the frame must be carefully ... ... and mounting the frame inside the rack ... Once the frame is secured in ... ... ) SYAFSU8 - Symmetra LX top panel ... ) SYAFSU6 - Symmetra LX castors ( ... ... ) SYAFSU7 - Symmetra LX castors ( ... ... ) syafsu10r - Symmetra LX 19U right ... ... ) syafsu10l - Symmetra LX 19U left ...
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX; What ... maximum number of XR frames allowed with a Symmetra PX solution? Symmetra PX 20, ... ... maximum number of XR frames allowed with a Symmetra PX solution is ... ... size of the Symmetra PX Main Frame . For a Symmetra PX 20 or 40kw Frame , the maximum ... fully populated ( Battery Frames) XR frames. The Battery Monitoring Card cannot ... of addresses for XR frames. ... a fully populated XR frame is SYCFXR8- ... ... consists of the XR frame with 8 Batteries Modules.
How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame?
Issue How can I extend the cable length of a Symmetra LX or Symmetra RM XR battery frame ?
Stacking limitations for single phase Symmetra and Matrix products
... the single phase Symmetra and Matrix family ... Symmetra and Matrix UPS Symmetra LX products in ... When stacking Symmetra LX products, ... ... 8kva or 16kva Symmetra LX chassis using ... ... stacking options, APC always recommends the ... APC offers Symmetra LX Tower systems with integrated XR battery cabinets (ex ... ... before purchasing the Symmetra LX UPS. Symmetra Power Array Products ... ... The UPS and batteries can be stacked ... 3 syxr4's can also ... ... SYXR12 12- Battery XR Cabinet or SYMSTRF ... The UPS and batteries can be stacked 36.6"" high. ... 1 mx3000pe/mx5000pe on bottom, 2 Smartcells (not XRs ) on top


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.