Browse FAQs



Symmetra Power Array Input Voltage Selector Theory of Operation
... for two things: routing power through the appropriate taps of the isolation transformer and notifying the intelligence modules of the expected input voltage.
Where can I get support for APC and MGE Products?
For support on APC and MGE products please visit: http://www. apc .com/support/ ... APC CS APC Enterprise Manager APC ES APC RS ... Microsol Modules Isoladores ... Step-Down Transformer ... Symmetra Power Module
Description of Galvanic Isolation
The actual benefit of installing an isolation transformer is that common mode noise fed to the computer is greatly reduced. Common mode noise can also be reduced by using noise filters, such as in the APC Smart-UPS series. The filters can work as well as the isolation transformer , especially at high frequencies where computers and networks operate. The isolation transformer is better at very low (audio) frequencies.
Powerview displays Rev. N, please wait or does not communicate with the UPS
If the UPS is a Symmetra LX, connect the PowerView to the other intelligence module to test a different pass-through port. ... Now that the accessories are communicating with a different intelligence module , observe if communication is re-established. ... If the problem cannot be isolated to a particular component and replacement of the parts mentioned above do not remedy the situation, there could be an issue with the backplane PCB of the Symmetra. If assistance is required with these troubleshooting steps, contact APC by Schneider Electric technical support.
How to navigate through an Network Air FM unit display
... commissioning of the Modules in the System ... ... apply to your APC NetworkAIR FM DX ... ... installed in the Modules of this System ... ... Input/Output Modules (PCIOMs) ... ... to the Main Module . # Modules in Sys. ... the number of Modules in this System ... ... Up to three Modules can be joined ... ... installed in the Modules of this System ... ... pattern for the Modules in this System ... Module Rot. ... Delays protect the Modules in the System ... ... ) in a Module engages. ... when an Expansion Module loses communication with the Main Module of a System ...
Steps to take when moving a Symmetra Power Array from one location to another
During the moving process be sure to remove ALL Power Modules and Battery Modules . The SYMIM (Main Intelligence Module ) and SYRIM (Redundant Intelligent Module ) can remain in the Symmetra Frame during shipping as long as the two securing thumbscrews are fastened prior to shipment. Due to the fact that the North American Symmetra Power Array has an Isolation Transformer built into the frame, the Symmetra MUST be shipped in an upright position.
Matrix-UPS frequently asked questions regarding installation, operation, and standards
This document provides the answers to commonly asked questions regarding installation of the APC Matrix UPS. ... 3. Set Matrix-UPS EU (Electronics Unit, the top half of the unit) in place on top of Matrix-UPS IU ( Isolation Unit, the bottom half of the unit) and tighten rear knob. ... This sound will be heard anytime the transformer is energizing (usually on startup) and is normal. The physical size of the transformer and the initial current surge into it causes this sound. ... APC Part Number
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
APC Boot Monitor apc _hw05_ ... 108.bin APC Operating System (AOS) apc _hw05_ ... .bin Application Module apc _hw05_ ...
PCNS log filling with "module added" and "module removed" events when in use with a single phase Symmetra
All currently released intelligence modules sold by APC by Schneider Electric run a firmware revision greater than 135.
APC KVM Switches and Corresponding Cables/Server Modules
APC KVM Part Numbers and Corresponding Cables/Server Modules ap5630 APC KVM PS/2 Server Module AP5631 APC KVM USB Server Module


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.