Browse FAQs



Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
... far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes ...
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Steps to take when moving a Symmetra Power Array from one location to another
... case you need to either send any components back to the APC or if you plan on moving your UPS in the future.
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
UPS & PDU Advantage Plus: See attached file; ARUO-ACQK4F_R7_EN_ Advantage Plus ... 1 Annual PM Visit ... UPS & PDU Advantage Prime: See attached file; ARUO-ACQGSD_R7_EN_ Advantage Prime ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra : See attached file; ARUO-ACQFVH_R6_EN_ Advantage Ultra ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable
Adding External Batteries to an SU, SUM, SURT, SURTA, SURTD or SUA series Smart-UPS XL
... as "" 1 "" within ... - Each unit counts as " ... ... or UXA Series Ultra Battery Packs - Each unit counts as " ... ... , some SURT units may ... battery as number 1 . (IE ... An surt3000xlt + 1 External Battery would ... On these units ""0 ... ... to set your unit to "" ... be "" 1 "". ... to set your unit to "" ... All other Smart-UPS count the internal battery as 0. (IE: An sua3000xl + 1 External Battery would be set to 1 )
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... Assessment Services ... Battery Replacement Services ... Environmental Monitoring Unit ... Installation Services ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Planning Tools and Publications ... Power Distribution Units ... Project Management Services ... Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Training Services
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... Sharing groups you plan to have. ... " port of one of the grouped ... This unit will be the ... ... powering up the units for the first ... desired order, 1 to 4. ... ... power up the unit that you would ... have Display ID 1 . After that unit has initialized and ... power on the unit that you would ... same way for units 3 and 4 ...
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) ... CM 003 ( 1 T) ... -230/ 1 /60 ... =277/ 1 /60 1 -5T ... 1 -3T ... ... -230/ 1 /60 ... =277/ 1 /60 ... CM 15 ( 1 T) ... =208/ 1 /60 ... =230/ 1 /60 ... =277/ 1 /60 ... Condenser/Condensing Unit (Not Current ...
What are the typical uses for an EcoAisle System
The efficiency gains in the cooling system when the EcoAisle is deployed reduce the number of cooling units in the solutions. ... The EcoAisle can easily be retrofitted into existing datacenters, allowing greater cooling capacities without adding more cooling units . ... Capacity Planning ... ‚óŹ 1 U Servers
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... , Environmental Monitoring Units (ap9320, ... Rack Air Removal Unit , PDPMXXX Modular ... ... , RACSCXXX Cooling Units (except ... , g50 AV Units , Smart- ... , acrc301s Cooling Units , ... who uses any one of the products ... One such example is ... ... future firmware update plans to address this ... ... ap9320 Environmental Monitoring Units ... Network Management Card 1 (NMC1) ... Rack Air Removal Unit AOS v3 ... ... a value of 1 to allow fallback ... Network Management Card 1 (NMC1) Information Bulletin: Effects ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.