Browse FAQs

Video: How to change the temperature thresholds on a Network Air FM unit

Published date: 16 October 2019

Issue:
This document contains a video on how to change the temperature thresholds on a Network Air FM unit.
 
Product line:
FM35-50, ACFM, IR40.
 
Environment:
All Serial Numbers.
 
Cause:
Install Operation.
 
Resolution:
 

How to change the temperature thresholds on a Network Air FM unit follow the below procedures. 
1 Press ESC until you reach the main menu (On/Off).

2 Scroll to SETUP and press ENTER.
 
3 Scroll to SYSTEM 1 and press ENTER.
 
4 Press ENTER on ALARMS.
 
5 Press ENTER on TEMPERATURE THRSHLD.
 
6 Select which threshold you want to change and then press ENTER.
 
7 Use the UP or DOWN arrows to select the desired temperature.
 
8 Press ENTER when finished.
 
9 Press ESC until you get back to the status screen.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.