Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. All Product models , all serial ... ... FM Air/ Water /Glycol Model W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... -230/ 3 / 60 ... = 480/ 3 / 60 ... = 600/ 3 / 60 E= Electric ... W= Hot Water U= Upflow R= Upflow Model A= 3 row 20 ... coil C= Chilled Water ... -230/ 3 / 60 ... = 480/ 3 / 60
What are the operational conditions for an InRoom (Stulz) Unit
... / 3ph / 60 Hz ... / 3ph / 60 Hz ... imbalance: < 3 % Frequency: 60 Hz +/ ... Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the ... cooled condenser: 60 m (200 ... ... condenser and the cooling unit: 5 ... is below the cooling unit ... evaporator capacity ( DX ): 24 ... Entering water temperature (EWT ... Leaving water temperature (LWT ... ... condensing temperature: 60 °C ( ... Cooling fluid ( DX ): 30 ... Chilled water medium (CW ...
How to navigate through an Network Air FM unit display
... APC NetworkAIR FM DX Precision Air Conditioner ... DX ... Direct expansion ( DX ) coil ... —Economizer and DX coils ... MultiCool® ( chilled water ) and DX coils ... , then the cooling setpoint is used ... ... the NetworkAIR FM DX 60 Hz Up to three Modules can be ... Water ... avoid over- cooling while dehumidifying. ... valve which feeds three quarters of the ... ... the modes ( cooling , reheat, ... ... the NetworkAIR FM DX 60 Hz Installation ... the NetworkAIR FM DX . ... for fluid- cooled options ... of fluid- cooled option.
What is the FM Water Flow Switch Alarms description?
FM Water Flow Switch Alarm ... Data Center Cooling ... If the flow switch is open and the MC/CW valve is a 3 way valve then an alarm will be generated. ... If you have selected a flow switch = DX /ECON If the flow switch is open and [the coil configuration = ECON or the water regulation valve = 3 way or (the water regulation valve = 2 way and the water regulation valve is open more than 30%)] then an alarm is generated.
Uniflair Humidifier Water Quality
Uniflair Humidifier Water Quality. Data Center Cooling . ... electrodes in the water generates the heat ... to boil the water and the amperometric ... ... closing the feed water solenoid valve and ... ... , the feed water solenoid valve is ... The cylinder electric drain valve is opened at intervals depending on the characteristics of the feed water supply in order to maintain the optimum concentration of dissolved minerals in the water in the cylinder. Feed water Values for the feed water for medium-high level of conductibility of a humidifier with immersed electrodes: ... ) 100 Temporary hardness mg/l 60 ( 3 ... ( 3
AirFlow CCT CW to DX Change Over
NOTE : Attached are documents regarding External Chilled Water Supply (ECWS) and its operation.
acrp100 Tech Data Manual
acrp100, acrp101, acrp102, acrp500, acrp501, acrp502, Tech DataManual, ACRP, Inrow, DX , Chilled Water
Video: How to reset an Air Filter Run Hours violation alarm on a Uniflair Unit
Uniflair, run, hours, violation, Chilled water , DX , Expansion, Direct
What is the IP (ingress or international protection) rating of SMC, SMT and SMX series Smart-UPS?
Other models of Smart- ... ... SMT and SMX models have been tested ... ... against solid objects greater than 12 mm ... offer protection against water . ... against solid objects greater than 50 mm ... against solid objects greater than 12 mm 3 = Protects against solid objects greater than 2. ... ... against solid objects greater than 1. ... ... harmful ingress of water . 1 = Protects against dripping water 2 = Protects against dripping water of +- 15 degree angle 3 = Protects against spraying water of +- 60 degree angle 4 = Protects against splashing water 5 = Protects against water jets
Where are your NetworkAIR ACFM manuals?
NetworkAIR FM DX , Precision, CRAC, Perimeter, ... acfm200, acfm400, Air-cooled, Water - cooled , Glycol- cooled


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.