Browse FAQs



NetBotz 450/550/570 | Physical Description
NetBotz version 3 - Rack Monitor 450 (451)
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... such as a Rack PDU, AV ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... Network Management Card 3 - ap9640, ... ... enhancements, bug fixes , or new ... ... Network Management Card 3 Symmetra 3 phase (Symmetra ... ... UPS or device type . ... Management Card v 3 .X. ... ... AP9619 use firmware 3 .X and ... ... application for your type of device. ... AP9635, and Rack PDU 2G ... 3 . From the ...
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... ... Network Management Card 3 (NMC3) ... ... UI, v 3 .X. ... Device Type ... Single or three phase Smart-UPS, Galaxy 3500, Matrix UPS ... Three phase Symmetra UPS (except 250/500kva & PX2) Symmetra 3 Phase APP or sy3p ... Rack Power Distribution Units Rack Power Distribution APP or rpdu ... Lastly, if the firmware upgrade does not resolve the issue, there may be a problem with the Network Management Card or the UPS SmartSlot.
Network Management Card 2 (NMC2) - snmpv1/v3 walk beginning at .iso through .iso.org.dod.internet does not work properly
An snmpv1/v 3 walk beginning at .iso through .iso.org.dod.internet does not work properly with my Network Management Card 2 device. ... Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... SNMP v1/v 3 ... This issue is resolved in AOS 6.1.2 or higher.
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
AP78XX Metered Rack PDU models, specifically ... The ( 3 ) load alarm thresholds are set incorrectly (Overload, Near Overload, and Low Load). You might find all three of these values are set to zero. Manually changing these values or resetting the unit to default settings should resolve this issue.
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
... Metered or Switched Rack PDU. ... and AP88XX Metered Rack PDUs ... Metered By Outlet Rack PDUs ... and AP86XX Metered Rack PDUs ... (AP79XX) Rack PDU's as well ... ) that have 3 .X. ... The problem that occurs stems from the Metered/or Switched Rack PDU and inline current meters reporting incorrect voltage. ... If you are experiencing this issue and need help fixing these values, please contact APC for assistance.
Do Not Enable Global Outlet Groups on Switched Rack PDUs (ap79xx) with 3.5.5 firmware
... of the Switched Rack PDU (AP79XX ... ... upgrade their Switched Rack PDU to firmware ... AP79XX Switched Rack PDU models ... .0- 3 .5. ... ... affects AP79XX Switched Rack PDUs. ... causes the Switched Rack PDU to become ... ... causes the Switched Rack PDU to become ... rpdu firmware v3.5.6 and higher solves this problem. ... This problem does not affect users with Metered Rack PDU's (AP78XX) due to the fact that this product line does not offer the Global Outlet Group feature.
Common Rack Automatic Transfer Switch Scenarios and Questions
... article discusses common Rack Automatic Transfer Switch ... Rack Automatic Transfer Switches ... All Rack ATS models listed ... As the Rack Automatic Transfer Switches ... INFORMATION BULLETIN - Upgrading Rack ATS Firmware (AP77XX) - potential to permanently damage ATS during download. ... ATS firmware v3.5.7 and higher aims to resolve this issue and will help prevent the ATS from tripping the upstream circuit breakers. ... Revise the voltage transfer range from medium to wide, revise frequency deviation from +/-2 Hz to +/- 3 Hz on the ATS: ... Using the Rack ATS with a Generator
Schneider Electric Rack LCD products and perceived "Image Burn In" / Dead Pixel Policy
Screen or image "burn in" on a Rack LCD product; appearance of a "ghost" image ... Rack LCD Console models: ... To enable this, press F 3 and configure the SCREEN BLANK:OFF(0) option to between 1-30 minutes. ... Schneider Electric's dead pixel policy requires at least (4) dead pixels in order to be covered under the two year repair or replace factory warranty.
NetBotz v3 | How do I manage user credentials and login alerting?
... on a version 3 NetBotz appliance. NetBotz v 3 Wall Appliance: 355/356 (nbwl0355/6) & 455/456 (nbwl0455/6) NetBotz v 3 Rack Appliance: 450/451 (nbrk0450/1), 550 (nbrk0550), & 570 (nbrk0570) ... NetBotz v 3 (all versions) ... 3 ) Under Appliance Settings ... 3 ) Click OK ... 3 ) Chose a Privilege Set ... The user can also resolve alert conditions for thresholds that are configured with the Return-To-Normal Requires User Input setting in their Advanced Settings.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.