Browse FAQs



Why Node-red embedded with Ecostruxure Augmented Operator Advisor stop few second after starting?
How to diagnotic When you start AOA, there is one MS-dos windows with a lot of information
LDAP/LDAPS Configuration with KVM1116P, KVM2116P, and KVM2132P Digital IP KVM Switches
... /LDAPS with Digital IP KVM Switches KVMXXXX Digital IP KVM Switches ... 1 . Install the Windows Server Support Tools ... 1 . On your Windows Server CD, open the Support >Tools folder. ... 3. Follow the Installation Wizard to complete the procedure. ... 1 . Open a Command Prompt. ... 1 . Right click Start. ... 1 . Create a new attribute. ... 1 . From the Start menu, open Administrative Tools > Active Directory Schema. ... The x500 Object ID must be unique ... 1 . Open the Control Panel > Administrative Tools > Active Directory Schema. ... 1 . Run ADSI Edit. ... CN=Users node .
Data Center Expert | What virtualization environments are supported?
... the Data Center Expert virtual appliance? ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all verisons ... ... found within the EcoStruxure IT Help Center ... ... -Center- Expert -Virtual- ... ... The Data Center Expert v7. ... The full-featured demo of the virtual appliance monitors up to five device nodes and one surveillance node . You can purchase a license key to upgrade to a production version to monitor additional device nodes and activate supported applications, or to migrate from a server hardware version to a virtual appliance.
Data Center Expert | How do hardware and software support contracts work?
... StruxureWare Data Center Expert Appliances can have ... total of 5 years , which includes 2 years of factory warranty ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 ... ASMNS5_R 1 _EN. ... ... amount of Device Nodes Installed 1 ) Open the Data Center Expert Desktop Client. ... ... all of the Node Count (column ... StruxureWare Data Center Expert Device Pack. 1 ) A Base ... the base 25 nodes installed on the ... 1 Year Software Support SKU 3 Year Software Support SKU
Creating an Aggregate Device within the KVM Access Software
... ships with KVMXXXX Digital IP KVMs) ... wishing to consolidate nodes within their KVM ... ... ports into a single Aggregate Device, ... counts as a single node , and only requires a single license. ... I have 300 node license but have ... ... purchase a 900 node license to cover ... effectively creating 150 nodes in total. ... ... the amount of nodes I need to ... 1 .) Within ... ... you are adding one of the specifically ... ... information under certain single sign on situations ... ... click on the one (s) ... ... device only has one network interface, ...
NetBotz 455 | Physical Description
- Flashing one very four seconds ... ... , displays the unique identifier number for one minute. 1 Microphone jack Supports ... ... humidity sensors with digital displays. 4 10/ 100 Base-T network port Provides for a 10/ 100 Base-T network connection and power through Power-over-Ethernet (PoE). (The appliance operates at 100 Base-T only.) Status and link LEDs indicate network traffic: ... - Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps).
NetBotz 250 | Physical Description
Ports for the handle sensors (NBHN125 or NBHN1356) on doors # 1 and #2. ... 9 10/ 100 Network Port Provides the connection to the network. ... 10 A-Link Ports Used to cascade NetBotz Rack Sensor Pod 150s (nbpd0150), or connect Temperature/Humidity Sensors with Digital Display (ap9520th).
NetBotz 750 | Physical Description
1 AC line inlet ... ... humidity sensors with digital displays) over ... 8 10/ 100 /1000 Network Port Provides a connection to the network. ... 9 Private LAN Provides a 10/ 100 /1000 connection to a private local area network and 48 VDC to an attached device. ... 13 Voltage Output Provides 12 VDC or 24 VDC (75 mA) to one connected device.
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... previous server already has licensing on it (beyond the base 25 device nodes and 1 surveillance node ) your will need to log into ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.