Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
StruxureWare Data Center Expert Appliances can have hardware warranty up to a total of 5 years , which includes 2 years of factory warranty.
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... to gather specific information about the alert ... 1 . In a ... 5 . To add ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine
Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an error ... StruxureWare Data Center Expert (DCE) ... StruxureWare Central (SWC ... StruxureWare Client (potentially ... StruxureWare may be attempting ... 1 ) Navigate to the Installation directory for StruxureWare Data Center Expert . (default directory is: C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X.X) ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe" 5 ) Save the file and open the client.
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
A single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... output of a single register for StruxureWare is a 16 ... ... handled by a single register. ... as 6553. 5 . ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... ... value of either 1 or 2. ... ... , the polling software must be reconfigured ... 31000 returns 0000000000000001 If this were a single register, = 1 ... This math must all done on the side of the querying application .
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
How to copy files from the StruxureWare Data Center Operation ... StruxureWare Data Center Operation ... StruxureWare Data Center Operation (All Versions) ... In this document, we will be using a free program called WinSCP. You can find this program . ... 1 . Open the application ... 5 . Using the "Arrow up button" to navigate up a directory, continue click the icon until the directory window reads / ... 1 . Double click on data folder ... 1 . Double click on /tmp folder
StruxureWare Data Center Expert shows duplicate sensors with values as "Unplugged" for NetBotz 750/755
When a NetBotz 5 discovers devices plugged into it or into ... into it, each device is given a unique identifier in the database.
Battery Age and UPS Age shown incorrectly in StruxureWare Data Center Expert.
Battery Age and UPS Age shown incorrectly in StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert 7.x ... Battery Age and UPS Age can have 5 different date formats on newer firmware. 1 : mm/dd/yyyy ... StruxureWare DCE may not show these formats correctly. ... file should be extracted and added to StruxureWare DCE.
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
How to change a RAID battery on the StruxureWare Data Center Expert Enterprise server?
... battery on the StruxureWare Data Center Expert Enterprise server? StruxureWare Data Center Expert StruxureWare Central StruxureWare Data Center Expert all versions ... configuration of the StruxureWare Data Center Expert Enterprise server is ... ... a Raid- 5 configuration that has ... This battery is crucial for high data integrity. ... 1 Pull back gently on the right edge of the battery bay and draw out the RAID battery from the battery carrier. ... 1 Connect the battery cable to the connector on the battery. ... See Figure 3- 1 . ... 5 If not already done, route the battery cable through the right chassis wall.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.