Technical FAQs

Ask a Question

What functionality does the LDAP feature provide on the NetBotz 750?
Issue: What functionality does the LDAP feature provide on the NetBotz 750? Product Line: NetBotz Environment: NetBot version 5x rack access LDAP...
StruxureWare Data Center Expert (DCE): Download the Essential Device Definition File (DDF) for NetBotz Rack Monitor 750
Issue: You cannot use the Web UI password to download the essential Device Definition (DDF) file for the Rack Monitor 750 in StruxureWare Data Center...
Local NetBotz Camera Pod 165 Does not Appear in the Appliance Web UI
Issue: If you move the camera pod from your company network (a remote connection) to the appliance’s private network (a local connection), the camera...
Video: How to install PowerChute Business Edition versions 9.0 to 9.2.1
Issue: How to install PowerChute Business Edition UPS monitoring software  Product: PowerChute Business Edition versions 9.0 to 9.2.1 Environment:...
NetBotz 250 | Inaccurate Data Logs (prior to v6.4.6 firmware)
Issue: On the NetBotz 250, temperature and humidity readings may show inaccurate readings in the data log, even though the correct readings are shown...
NetBotz v3 | Unplugged Sensor Alarm
Issue: There is an active alarm on a NetBotz appliance for an unplugged sensor. Product Line: NetBotz v3 (355, 455, 450, 550, & 570) Environment:...
Data Center Expert | API Information
Issue: StruxureWare Data Center Expert Application Programming Interface (API) Information Product Line: StruxureWare Data Center Expert (DCE) Environment: ...
What Proximity Cards are supported by the NetBotz NBACS125 & NBACS1356 Rack Access Control Systems?
The NBACS125 Rack Access Control appliance supports the following Proximity Cards H10301 - Standard 26 Bit H10302 - 37 Bit without facility code H10304...
ACRC Tech Data Manual
Issue:  ACRC Tech Data Manual Product line:  ACRC500, ACRC501, ACRC502 Environment:     Cause:    Tech Data Manual Resolution:   See file below
Video: Back-UPS ES "M"; Connecting computer data cable for Graceful Unattended Shutdown.
Issue: APC Back-UPS "M" ; Connecting computer data cable. BE425M / BN450M - User Manual BE600M1 / BN650M1 - User Manual BE850M2 / BN900M - User Manual...
Results 1 - 10 of 100