NetBotz Output Relay Label changes back to default after reboot
Published date:
20 July 2020
Issue:
NetBotz Output Relay Label changes back to default after reboot.
Product Line:
NetBotz
Environment:
NetBotz version 4.6.4 and earlier
Cause:
NetBotz Output Relay "Port Label" changes back to the default "Output(1)" or "Output(2)"
Resolution:
This issue has just recently been discovered in BotzWare version 4.6.4 and a few earlier revisions and should be fixed in an upcoming release.
In the meantime as a workaround, you can create a custom button type that is more descriptive. Normally the sensor would read something like:
"Switch (My Port Label)"
which after reboot, would change back to
"Switch (Output(1))"
If you add a custom switch or button type, you can leave the port as Output(1) and create a custom switch with a "Default Relay Output Label" something like the following:
"My Switch Output"
This would show up in the sensor view as:
"My Switch Output(Output(1))"
This configuration will survive a reboot.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.