Netbotz 700 | Change in private LAN IP does not fully update.
Published date:
21 July 2020
Issue:
NetBotz 750 Private Lan IP change fails to update
Product Line
NetBotz 700 Series
- NetBotz Rack Monitor 750 (NBRK0750)
Environment
NetBotz 700 Series (all versions)
Cause: When you configure a NetBotz appliance with a 172.x.x.x IP address, the private LAN should automatically reconfigure itself to a 192.168 address. Due to a defect, this caused the appliance to not detect the conflict and not switch the private network to the alternate subnet. Subsequent response traffic is sent to the wrong interface resulting in browser timeouts and other issues.
Resolution:
For the time being, we recommend not adding the NetBotz 750 /755 to a network in this range. This issue is scheduled to be resolved in the next release of the NetBotz 750 firmware, 5.2.2.
Should this be a requirement, please contact technical support to obtain a patch.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.