Browse FAQs

What VMware ESXi Licenses are support with PowerChute?

Published date: 12 August 2020

Issue:
PowerChute can only shutdown full licensed ESXi hosts.

Product Lines:
PowerChute Network Shutdown
PowerChute Business Edition

Environment:
VMware ESXi versions, 4.x, 5.x, 6.x

Cause:
  1. VMware restricts RCLI (remote command line interface) administration access for the free version of ESXi (no write access). 
  2. This is an issue with the remote command line interface (RCLI).
Solution:
Purchase VMware Essentials, Standard, Enterprise, Enterprise Plus License http://www.vmware.com/products/vsphere/pricing

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.