Browse FAQs

What alarms can be automatically reset on a High Capacity Uniflair Unit

Published date: 18 July 2020

Issue:  
This article contains what alarms can be automatically reset on a High Capacity Uniflair Unit.

Product line:
High capacity Models 4500/5000.

Environment:  
All Serial Numbers. 

Cause:  
Install.  

Resolution:

The Automatic Reset allows the unit to clear the alarm and continue operation if the alarm condition is no longer present.

 

• High/Low Temperature Threshold Exceeded

• High/Low Humidity Threshold Exceeded

• Supply Air Temperature Threshold Exceeded

• High/Low Airflow

• Humidifier

• Smoke Detected

• Electric Heater Over Temperature

• Electronic Expansion Valve Error

• Low Pressure

• Circuit 1 Chilled Water High Temperature Threshold Exceeded

• Circuit 1 Chilled Water Temperature too High for Dehumidification

• Insufficient Chilled Water Flow

• Primary/Secondary Power Source Unavailable

• Dual Circuit Expansion Board Error Detected

• Digital 2/4/6 Input Abnormal

• External Sensor Threshold Exceeded

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.