Browse FAQs

Data Center Expert | Using APC SNMP Device Configuration to change SNMP settings may disassociate the current notification policy for that device.

Published date: 06 May 2021

Issue
Changing SNMP settings for APC Devices using APC SNMP Device Configuration within Data Center Expert may cause the device to be disassociated from its current notification policy.

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment
StruxureWare Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)

Cause
Switching the protocol used for communication between Data Center Expert and APC Devices from SNMPv1 to SNMPv3 may disassociate the current notification policy.
Mass configuring APC Device SNMP settings using APC SNMP Device Configuration within Data Center Expert may disassociate the current notification policy.


Resolution:

After using APC SNMP Device Configuration, for an SNMP settings change or a migration from SNMPv1 to SNMPv3, check the notification policies and ensure the correct devices are listed within each of them.  If a device has reset to the Default notification policy, ensure to move it to the correct notification policy. This will need to be done manually for each device.

This has been resolved in DCE 7.8.1
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.